This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:tools:m1k:alice:desk-top-awg-users-guide [22 Oct 2020 16:00] – [Custom Math Waveforms] Doug Mercer | university:tools:m1k:alice:desk-top-awg-users-guide [09 Jul 2021 22:42] (current) – [AWG Controls Window:] Doug Mercer | ||
---|---|---|---|
Line 33: | Line 33: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Wave Shapes below the line separator in the menu use the AWGAwaveform or AWGBwaveform array buffers to contain the waveform sample data points. A new data set based on the entered values is generated each time the button is clicked. The Impulse, Trapezoid, U-D Ramp, UU Noise ( uncorrelated uniform distribution ) and UG Noise (uncorrelated | + | Random " |
+ | |||
+ | Wave Shapes below the line separator in the menu use the AWGAwaveform or AWGBwaveform array buffers to contain the waveform sample data points. A new data set based on the entered values is generated each time the button is clicked | ||
+ | |||
+ | The Impulse, Trapezoid, U-D Ramp, UU Noise ( uncorrelated uniform distribution ) and UG Noise (uncorrelated | ||
The basic shape of the Impulse waveform is shown in figure 10. The Max, Min, Freq, Phase and Duty-Cycle values are used to construct the waveform. The Freq setting determines the Period ( 1/Freq ) or spacing between the pulses. The output starts and ends at a value midway between the Min and Max values. The impulse consists of a positive peak followed by a negative peak. The width of the peaks are equal to (Period * DutyCycle)/ 2. The center of the pulse is delayed by the Phase setting. For example if the phase is set to 180 then the pulse is delayed by ½ the Period (Phase/ | The basic shape of the Impulse waveform is shown in figure 10. The Max, Min, Freq, Phase and Duty-Cycle values are used to construct the waveform. The Freq setting determines the Period ( 1/Freq ) or spacing between the pulses. The output starts and ends at a value midway between the Min and Max values. The impulse consists of a positive peak followed by a negative peak. The width of the peaks are equal to (Period * DutyCycle)/ 2. The center of the pulse is delayed by the Phase setting. For example if the phase is set to 180 then the pulse is delayed by ½ the Period (Phase/ |