This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
university:tools:m1k:alice:advanced-equivalent-time-sampling-guide [30 Apr 2020 16:21] – created Doug Mercer | university:tools:m1k:alice:advanced-equivalent-time-sampling-guide [27 Jan 2021 22:37] (current) – use wp> interwiki links Robin Getz | ||
---|---|---|---|
Line 77: | Line 77: | ||
To convert back to the actual sample rate: | To convert back to the actual sample rate: | ||
- | Actual Sample Rate = int(round((1.0 / sample_time) / 2.0)) | + | Actual Sample Rate = int(round( (1.0/ |
The first possible sample rate lower than the 100 KSPS maximum is 99585. The next below that is 99174, and below that is 98765, 98361 etc. These values are doubled of course when sampling just 2 channels. These are small but still finite steps in the available sample rates. | The first possible sample rate lower than the 100 KSPS maximum is 99585. The next below that is 99174, and below that is 98765, 98361 etc. These values are doubled of course when sampling just 2 channels. These are small but still finite steps in the available sample rates. | ||
Line 139: | Line 139: | ||
====Input Frequency Compensation==== | ====Input Frequency Compensation==== | ||
- | The software frequency compensation for each channel consists of a cascade of two adjustable [[https:// | + | The software frequency compensation for each channel consists of a cascade of two adjustable [[wp>High-pass_filter# |
This functionality is generally used to compensate for a low pass response that might be introduced when using external resistor dividers and the internal input capacitance of the ALM1000 AIN and BIN pins. These software frequency compensation filters can also be used to compensate for the internal 100 KHz anti-alias filter in the ETS mode. Based on the time scale multiplication factor appropriate time constant and gain factors can be calculated from fixed values for any given multiplier. | This functionality is generally used to compensate for a low pass response that might be introduced when using external resistor dividers and the internal input capacitance of the ALM1000 AIN and BIN pins. These software frequency compensation filters can also be used to compensate for the internal 100 KHz anti-alias filter in the ETS mode. Based on the time scale multiplication factor appropriate time constant and gain factors can be calculated from fixed values for any given multiplier. |