This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:labs:comms_lab_transformers_adalm2000 [18 May 2020 17:56] – ↷ Page moved and renamed from university:labs:m2k:comms_lab_transformers to university:labs:comms_lab_transformers_adalm2000 Cristina Suteu | university:labs:comms_lab_transformers_adalm2000 [18 May 2020 18:00] – media files from current location Cristina Suteu | ||
---|---|---|---|
Line 13: | Line 13: | ||
The transformer core has high magnetic permeability, | The transformer core has high magnetic permeability, | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 87: | Line 87: | ||
I< | I< | ||
- | ====Pre Lab Simulations==== | + | ====Pre Lab Simulaations==== |
Before measuring the frequency response of the transformers supplied in your parts kit, create a simulation schematic similar to figure 2 and perform an AC sweep from 10 KHz to 10 MHz. Use the manufacturer' | Before measuring the frequency response of the transformers supplied in your parts kit, create a simulation schematic similar to figure 2 and perform an AC sweep from 10 KHz to 10 MHz. Use the manufacturer' | ||
Line 102: | Line 102: | ||
Build the circuit shown in figure 2 on your solder-less breadboard. You will be using this setup to measure the frequency response of each of the two transformer model numbers in three different configuration with 1:1 primary to secondary turns ratios. The two red arrows indicate where to connect the source and load resistors for the configuration where one coil is used for the primary and secondary. The blue arrows are for the configuration where two coils in series are used for the primary and secondary. The green arrows are for the configuration where three coils in series are used for the primary and secondary. | Build the circuit shown in figure 2 on your solder-less breadboard. You will be using this setup to measure the frequency response of each of the two transformer model numbers in three different configuration with 1:1 primary to secondary turns ratios. The two red arrows indicate where to connect the source and load resistors for the configuration where one coil is used for the primary and secondary. The blue arrows are for the configuration where two coils in series are used for the primary and secondary. The green arrows are for the configuration where three coils in series are used for the primary and secondary. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 114: | Line 114: | ||
=====Procedure: | =====Procedure: | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 128: | Line 128: | ||
Connect to the transformer for a 1:2 step up configuration (red arrows) and a 2:1 step down configuration as shown in figure 3. | Connect to the transformer for a 1:2 step up configuration (red arrows) and a 2:1 step down configuration as shown in figure 3. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 134: | Line 134: | ||
Use the impedance matching formula to calculate the appropriate value for R< | Use the impedance matching formula to calculate the appropriate value for R< | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
=====Procedure: | =====Procedure: | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> |