This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
university:labs:comms_lab_isr_adalm2000 [18 May 2020 17:41] – ↷ Page moved and renamed from university:labs:m2k:comms_lab_isr to university:labs:comms_lab_isr_adalm2000 Cristina Suteu | university:labs:comms_lab_isr_adalm2000 [18 May 2020 17:50] – media files from current location Cristina Suteu | ||
---|---|---|---|
Line 9: | Line 9: | ||
The inductors supplied in your parts kit, like all non-ideal electrical components, are not perfect. The schematic in figure 1 shows the most common simple model of a real inductor. In addition to the desired inductance L, the real component also has loss ( modeled as a series resistance, shown in the schematic as R ) and a parallel parasitic capacitance, | The inductors supplied in your parts kit, like all non-ideal electrical components, are not perfect. The schematic in figure 1 shows the most common simple model of a real inductor. In addition to the desired inductance L, the real component also has loss ( modeled as a series resistance, shown in the schematic as R ) and a parallel parasitic capacitance, | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 43: | Line 43: | ||
The schematic in figure 2 shows the simulation test circuit for the three element LRC model of the inductor. L, R and C< | The schematic in figure 2 shows the simulation test circuit for the three element LRC model of the inductor. L, R and C< | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 51: | Line 51: | ||
Two frequency sweep simulations were run from 10KHz to 10MHz as an example of a 1mH inductor, L, with C< | Two frequency sweep simulations were run from 10KHz to 10MHz as an example of a 1mH inductor, L, with C< | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 66: | Line 66: | ||
Build the Inductor test circuit as shown in figure 4 on your solder-less breadboard. The green squares indicate where to connect the ADALM2000 AWG and scope channels. | Build the Inductor test circuit as shown in figure 4 on your solder-less breadboard. The green squares indicate where to connect the ADALM2000 AWG and scope channels. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 73: | Line 73: | ||
The connections to the ADALM2000 AWG output and scope channel inputs are as indicated by the green boxes in figure 4. Your parts kit should contain a number of inductors with different values. Insert each inductor, one at a time into your test circuit. | The connections to the ADALM2000 AWG output and scope channel inputs are as indicated by the green boxes in figure 4. Your parts kit should contain a number of inductors with different values. Insert each inductor, one at a time into your test circuit. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 82: | Line 82: | ||
Run a single sweep for each inductor in your kit of parts. You should see amplitude and phase vs frequency plots that look very similar to your simulation results. Be sure to export the data to a .csv file for further analysis in either Excel or Matlab. | Run a single sweep for each inductor in your kit of parts. You should see amplitude and phase vs frequency plots that look very similar to your simulation results. Be sure to export the data to a .csv file for further analysis in either Excel or Matlab. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> |