This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:labs:cascaded_rc_adalm2000 [18 May 2020 17:28] – ↷ Page moved and renamed from university:labs:m2k:cascaded_rc to university:labs:cascaded_rc_adalm2000 Cristina Suteu | university:labs:cascaded_rc_adalm2000 [18 May 2020 17:32] – media files from current location Cristina Suteu | ||
---|---|---|---|
Line 38: | Line 38: | ||
Build the circuit presented in figure 3 on the solderless breadboard. | Build the circuit presented in figure 3 on the solderless breadboard. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
====Procedure==== | ====Procedure==== | ||
In network analyzer you will do a logarithmic sweep. Set the start frequency to 100 Hz and the stop frequency to 20 KHz. The magnitude axis can be set to -50 dB minimum and 10 dB maximum. The phase axis goes from -180 to 90 degrees. | In network analyzer you will do a logarithmic sweep. Set the start frequency to 100 Hz and the stop frequency to 20 KHz. The magnitude axis can be set to -50 dB minimum and 10 dB maximum. The phase axis goes from -180 to 90 degrees. | ||
Run the network analyzer to obtain the frequency response plot of the RC filter. | Run the network analyzer to obtain the frequency response plot of the RC filter. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 52: | Line 52: | ||
====Hardware setup==== | ====Hardware setup==== | ||
Add a second RC low pass section to the prevoius filter as shown in Figure 6. | Add a second RC low pass section to the prevoius filter as shown in Figure 6. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
====Procedure==== | ====Procedure==== | ||
Keep the same parameters set in the network analizer. Put the oscilloscope channel 2 after the first RC stage and do a single sweep. This will be the reference sweep an can be kept on the plot by pressing the Snapshot button in the Reference section of the Network analizer General Settings. Move the oscilloscope channel 2 after the second RC stage and do another sweep. You should see on the plot the frequency response after both RC stages as in Figure 8. | Keep the same parameters set in the network analizer. Put the oscilloscope channel 2 after the first RC stage and do a single sweep. This will be the reference sweep an can be kept on the plot by pressing the Snapshot button in the Reference section of the Network analizer General Settings. Move the oscilloscope channel 2 after the second RC stage and do another sweep. You should see on the plot the frequency response after both RC stages as in Figure 8. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 65: | Line 65: | ||
====Hardware setup==== | ====Hardware setup==== | ||
As a further extension of this cascade of RC low pass filter sections add a third RC section to make a 3rd order filter by connecting another R and C to your circuit as shown in figure 9. | As a further extension of this cascade of RC low pass filter sections add a third RC section to make a 3rd order filter by connecting another R and C to your circuit as shown in figure 9. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
====Procedure==== | ====Procedure==== | ||
Keep the same parameters set in the network analizer. Put the oscilloscope channel 2 after the first RC stage ( point A shown in figure 10) and do a single sweep. This will be the reference sweep an can be kept on the plot by pressing the Snapshot button in the Reference section of the Network analizer General Settings. Move the oscilloscope channel 2 after the second RC stage (point B) and do another sweep and press the Snapshot button. You should see on the plot the frequency response after both RC stages. To obtain the frequency response of the third stage put the oscilloscope channel 2 in point C and do another sweep. You should see all three responses as in figure 11. | Keep the same parameters set in the network analizer. Put the oscilloscope channel 2 after the first RC stage ( point A shown in figure 10) and do a single sweep. This will be the reference sweep an can be kept on the plot by pressing the Snapshot button in the Reference section of the Network analizer General Settings. Move the oscilloscope channel 2 after the second RC stage (point B) and do another sweep and press the Snapshot button. You should see on the plot the frequency response after both RC stages. To obtain the frequency response of the third stage put the oscilloscope channel 2 in point C and do another sweep. You should see all three responses as in figure 11. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
\\ | \\ |