This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:eps:photovoltaic [19 Jul 2017 14:58] – [Directions:] Doug Mercer | university:courses:eps:photovoltaic [24 Jul 2017 16:16] – change amplitude value to peak-peak Antoniu Miclaus | ||
---|---|---|---|
Line 111: | Line 111: | ||
Set the frequency of waveform generator 1 to 20 Hz, and the horizontal time base so that at least one full 0 to V< | Set the frequency of waveform generator 1 to 20 Hz, and the horizontal time base so that at least one full 0 to V< | ||
- | Set the amplitude of waveform generator 1 to slightly more than 2.5V ( >5V peak to peak ). Depending on the V< | + | Set the amplitude of waveform generator 1 to slightly more than 5V. Depending on the V< |
===== Procedure: ===== | ===== Procedure: ===== |