Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
university:courses:eps:photovoltaic [24 Jul 2017 16:16] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:eps:photovoltaic [28 Apr 2019 14:55] – change to ALM2000 Doug Mercer |
---|
Scope channel 1 measures the solar panel voltage with input 1+ connected to the + terminal of the panel and input 1- connected to the - terminal of the panel. Scope channel 2 measures the current by measuring the voltage across 10 Ω resistor R<sub>1</sub> with input 2+ connected to the source terminal of M<sub>1</sub> and input 2- connected to the - terminal of the panel. | Scope channel 1 measures the solar panel voltage with input 1+ connected to the + terminal of the panel and input 1- connected to the - terminal of the panel. Scope channel 2 measures the current by measuring the voltage across 10 Ω resistor R<sub>1</sub> with input 2+ connected to the source terminal of M<sub>1</sub> and input 2- connected to the - terminal of the panel. |
| |
The configuration shown in figure 9 can measure only part of the I/V curve for panels with V<sub>OC</sub> greater than about 5V. It should be used to measure I<sub>SC</sub>for any panel. To measure the rest of the I/V curve for panels with V<sub>OC</sub> up to 10 volts the circuit can be modified as shown in figure 10. The waveform generator in the Discovery can swing a maximum of 10 Volts (-5 to +5) so that will be the ultimate limit of the total voltage range of any I/V measurements that can be produced using these setups. | The configuration shown in figure 9 can measure only part of the I/V curve for panels with V<sub>OC</sub> greater than about 5V. It should be used to measure I<sub>SC</sub>for any panel. To measure the rest of the I/V curve for panels with V<sub>OC</sub> up to 10 volts the circuit can be modified as shown in figure 10. The waveform generator in the ALM2000 can swing a maximum of 10 Volts (-5 to +5) so that will be the ultimate limit of the total voltage range of any I/V measurements that can be produced using these setups. |
| |
{{ :university:courses:eps:eps_photovoltaics-f10-r1.png?500 |}} | {{ :university:courses:eps:eps_photovoltaics-f10-r1.png?500 |}} |