This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
university:courses:eps:diode-curves [16 Jun 2013 03:53] – created Doug Mercer | university:courses:eps:diode-curves [21 May 2014 14:41] (current) – [Hardware Setup:] Doug Mercer | ||
---|---|---|---|
Line 54: | Line 54: | ||
q = electronic charge = 1.6 * 10< | q = electronic charge = 1.6 * 10< | ||
f< | f< | ||
- | k = Boltzman' | + | k = Boltzman' |
n = ideality factor (forward slope factor, determined by metal-semiconductor interface) | n = ideality factor (forward slope factor, determined by metal-semiconductor interface) | ||
Line 101: | Line 101: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 100 Hz triangle wave with 3 volt amplitude and 0 volt offset. The differential input of scope channel 2 (2+,2-) is used to measure the current in the resistor (and diode). The single ended input of scope channel 1 (1+) is used to measure the voltage across the diode (1- input is grounded). The Scope should be setup with channel 1 at 500mV per division and channel 2 set also at 500mV per division. The current flowing through the diode, I< | + | The waveform generator should be configured for a 100 Hz triangle wave with 3 volt amplitude and 0 volt offset. The differential input of scope channel 2 (2+,2-) is used to measure the current in the resistor (and diode). The single ended input of scope channel 1 (1+) is used to measure the voltage across the diode (1- input is grounded). The Scope should be setup with channel 1 at 500mV per division and channel 2 set also at 500mV per division. The current flowing through the diode, I< |
===== Procedure: ===== | ===== Procedure: ===== |