Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
university:courses:eps:diode-curves [20 May 2014 16:20]
Doug Mercer [Schottky Diode Fundamentals:]
university:courses:eps:diode-curves [21 May 2014 14:41]
Doug Mercer [Hardware Setup:]
Line 101: Line 101:
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-The waveform generator should be configured for a 100 Hz triangle wave with 3 volt amplitude and 0 volt offset. The differential input of scope channel 2 (2+,2-) is used to measure the current in the resistor (and diode). The single ended input of scope channel 1 (1+) is used to measure the voltage across the diode (1- input is grounded). The Scope should be setup with channel 1 at 500mV per division and channel 2 set also at 500mV per division. The current flowing through the diode, I<​sub>​D</​sub>,​ is the voltage measured by channel 2 divided by the resistor value (100 in this example). Use the XY display mode to plot the voltage across the diode (scope channel 1) on the X axis vs. the current in the diode (scope channel 2) on the Y axis.+The waveform generator should be configured for a 100 Hz triangle wave with 3 volt amplitude and 0 volt offset. The differential input of scope channel 2 (2+,2-) is used to measure the current in the resistor (and diode). The single ended input of scope channel 1 (1+) is used to measure the voltage across the diode (1- input is grounded). The Scope should be setup with channel 1 at 500mV per division and channel 2 set also at 500mV per division. The current flowing through the diode, I<​sub>​D</​sub>,​ is the voltage measured by channel 2 divided by the resistor value (100 Ω in this example). Use the XY display mode to plot the voltage across the diode (scope channel 1) on the X axis vs. the current in the diode (scope channel 2) on the Y axis.
  
 ===== Procedure: ===== ===== Procedure: =====
university/courses/eps/diode-curves.txt · Last modified: 21 May 2014 14:41 by Doug Mercer