This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:courses:engineering_discovery:lab_6 [04 Sep 2019 20:27] – [Materials and Apparatus] Doug Mercer | university:courses:engineering_discovery:lab_6 [04 Sep 2019 20:32] (current) – add alternate inductor options from kit Doug Mercer | ||
---|---|---|---|
Line 31: | Line 31: | ||
==== Procedure ==== | ==== Procedure ==== | ||
- Construct the following electromagnet circuit on the solderless breadboard{{ university: | - Construct the following electromagnet circuit on the solderless breadboard{{ university: | ||
- | - **Note that the 100 Ω resistors get very hot due to Joule heating, so avoid coming in contact with them** | + | - **Note that the 100 Ω resistors get very hot due to Joule heating, so avoid coming in contact with them** |
- Refer to the illustration below for one way to install the components in the solderless breadboard{{ university: | - Refer to the illustration below for one way to install the components in the solderless breadboard{{ university: | ||
- Add the following Hall effect sensor circuit to the solderless breadboard{{ university: | - Add the following Hall effect sensor circuit to the solderless breadboard{{ university: |