This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
university:courses:engineering_discovery:lab_4 [08 Apr 2016 21:57] – Jonathan Pearson | university:courses:engineering_discovery:lab_4 [08 Apr 2016 23:01] – Jonathan Pearson | ||
---|---|---|---|
Line 30: | Line 30: | ||
- Construct the following circuit on the solderless breadboard; note that the +5 V power is to be supplied by the M1K{{ university: | - Construct the following circuit on the solderless breadboard; note that the +5 V power is to be supplied by the M1K{{ university: | ||
- Refer to the illustration below for one way to install the components in the solderless breadboard; note that the top rows are reserved for 5.0 V and GND connections{{ university: | - Refer to the illustration below for one way to install the components in the solderless breadboard; note that the top rows are reserved for 5.0 V and GND connections{{ university: | ||
+ | - Refer to the included section below for details regarding the microphone pin assignments{{page>/ | ||
- Refer to the illustration below that shows how to connect the components{{ university: | - Refer to the illustration below that shows how to connect the components{{ university: | ||
- See the illustration below that shows how to connect an extension cable to the loudspeaker{{ university: | - See the illustration below that shows how to connect an extension cable to the loudspeaker{{ university: |