This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:engineering_discovery:lab_4 [08 Apr 2016 21:55] – Jonathan Pearson | university:courses:engineering_discovery:lab_4 [08 Apr 2016 23:01] – Jonathan Pearson | ||
---|---|---|---|
Line 9: | Line 9: | ||
==== Materials and Apparatus ==== | ==== Materials and Apparatus ==== | ||
* Data sheet handouts for OP484, electret microphone, and 2N3904 | * Data sheet handouts for OP484, electret microphone, and 2N3904 | ||
- | * Audio Amplifier Experiment article handout (linked below to a wiki version) | + | * Audio Amplifier Experiment article handout (linked below in the " |
* IC pinout handout | * IC pinout handout | ||
* Computer running PixelPulse software | * Computer running PixelPulse software | ||
Line 30: | Line 30: | ||
- Construct the following circuit on the solderless breadboard; note that the +5 V power is to be supplied by the M1K{{ university: | - Construct the following circuit on the solderless breadboard; note that the +5 V power is to be supplied by the M1K{{ university: | ||
- Refer to the illustration below for one way to install the components in the solderless breadboard; note that the top rows are reserved for 5.0 V and GND connections{{ university: | - Refer to the illustration below for one way to install the components in the solderless breadboard; note that the top rows are reserved for 5.0 V and GND connections{{ university: | ||
+ | - Refer to the included section below for details regarding the microphone pin assignments{{page>/ | ||
- Refer to the illustration below that shows how to connect the components{{ university: | - Refer to the illustration below that shows how to connect the components{{ university: | ||
- See the illustration below that shows how to connect an extension cable to the loudspeaker{{ university: | - See the illustration below that shows how to connect an extension cable to the loudspeaker{{ university: |