This is an old revision of the document!
VideoNumberHere
After mastering the basic operation of the M1K and PixelPulse application software, it is useful to show how to build simple circuits on the solderless breadboard, connect them to the M1K, generate voltages and currents, and measure voltages on the PixelPulse display. In this lab we initially show how the solderless breadboard is used to construct circuits. We then build a voltage divider and a current divider, each comprised of resistors, on the solderless breadboard, and show how the details regarding how to connect the ciruit to the M1K. Finally, we use a voltage source and current source in the M1K, controlled by PixelPulse software, to drive these circuits, and measure the voltages across the resistors on the computer display using the M1K and PixelPulse software.
To gain a basic understanding of how to use the M1K, PixelPulse software, and the parts in the ADALP2000 Analog Parts Kit to build circuits and perform experiments on those circuits. To understand how basic schematic symbols, such as those used to represent the circuit ground and power supply voltage, are interpreted when constructing and analyzing a real circuit. To understand how voltage and current divider circuits work and how to calculate individual voltages in voltage dividers and individual currents in current dividers. Following completion of this lab you should be able to explain the basic operation the M1K and PixelPulse software, how to construct circuits on the solderless breadboard for evaluation, and calculate all voltages and currents in voltage and current divider circuits.
This lab has two main purposes. The first is to become familiar with basic schematic symbols, with emphasis on “ground,” and how to convert them into real circuits that connect to real signal generators and analyzers. The second purpose is to build and analyze two simple circuits: a voltage divider comprised of resistors connected in series, and a current divider comprised of resistors connected in parallel. The voltage divider is fed by a voltage source and the current divider is fed by a current source. In the voltage divider we calculate and measure the voltage across the resistors and in the current divider we calculate the voltage across the resistors and the current through each resistor. We derive the “voltage divider rule” and “current divider rule” below.
The concept of “ground” in circuits can sometimes lead to confusion. Terms like “signal ground,” “earth ground,” “chassis ground,” “safety ground,” “single-ended,” “differential,” “balanced,” “common-mode,” “ground loops,” and many others get tossed around, often without a full understanding of their meanings. The basic concept of an ideal ground is introduced here and can be extended to any system, and imperfections in grounding systems can be understood and dealt with by modeling the grounding system with lumped and distributed circuit elements.
First it is necessary to emphasize that all voltages are differences in electrical potential between two distinct points. It therefore makes no sense to speak of a voltage at one point without referencing that point to another point. It is something like relative velocities. Two vehicles traveling in the same direction at the same speed are traveling at a velocity of zero with respect to each other, but may be traveling at 60 mph relative to the road. They are traveling at different velocities relative to the sun, and so on. The voltage between two battery terminals may be nominally 9 volts, but the voltage between one of the battery terminals and the terminal of a battery connected in another system is something else. In systems that use a ground reference, sometimes the fact that voltages are measured with respect to that ground is overlooked.
An ideal ground in a system has exactly the same voltage with respect to an ideal reference (equipotential) no matter where in the system that voltage is measured. All voltages within this system are measured with respect to this one ideal ground potential. A clear requirement of this ideal ground is that it have zero impedance such that any currents that flow within it do not develop voltage drops that would violate the equipotential requirement. This type of ideal ground is not realizable, but can be approximated using high quality conductors. At low frequencies the resistive component of ground impedance dominates, and at higher frequencies the skin effect increases resistance, and the inductive component of impedance begins to take effect. All of these produce undesirable voltage drops in the ground. There are many ways to implement grounds that are optimized for particular applications and signal frequencies that are well beyond the scope of this lab and any experiments that can be developed for the M1K. For our purposes, we can use an ideal ground approximation because the inductance in the ground is negligible due to the low signal frequencies encountered, and the ground interconnections have negligible resistance compared with the resistance levels encountered in the labs.
There are a number of different symbols used on schematic diagrams to represent different types of grounds. Some common types are shown below.{insert drawing when computer is back from IT}
When we see a particular ground symbol on a schematic drawing, we know that it represents one of the reference potentials that is used by our system. There may be many such ground symbols on the schematic, and we can envision these as all being connected together.
The solderless breadboard used with the M1K is comprised of a plastic block with a two-sided array of holes, with internal metal contacts, that are arranged in a grid. Each side of the array is made up of a series of five-hole rows, in which all of the metal contacts are connected together. This allows us to make circuit connections by placing the leads of the elements we wish to connect together in the same row. See the illustration below for an example{Place illustration here when PC is back from IT}
When constructing the labs on the solderless breadboard all ground connections indicated on the schematic should be connected together and to one or both GND ports on the M1K. We can view ground as our zero potential reference for all voltages generated and measured in the labs.
Series circuits are defined as circuits in which the same current flows through all elements. All of the elements carry the same current, but the voltage across a series circuit is divided among its series elements. For this reason, the series circuit is sometimes referred to as a voltage divider. We often need to know the voltage across a particular circuit element, and this can be easily calculated using the voltage divider rule, which only requires knowledge of the circuit element values and the voltage across the series circuit. We will use a resistive circuit to derive the voltage divider rule.
If we apply a voltage VT (T is for Total) across a series circuit comprised of resistors, as illustrated below, a current I flows in the circuit that is calculated using Ohm's law as
The voltage Vm across a particular resistor, Rm, is calculated as
If we substitute the current from the first equation into the second equation and solve for Vm we obtain the voltage divider rule:
The voltage divider rule for resistors therefore shows that the voltage across any resistor in a series connection is equal to the voltage across the series circuit multiplied by the ratio of the value of the resistor of interest to the sum of all of the resistances in the circuit. This ratio represents the percentage of the total voltage across the series circuit that appears across the resistor of interest. We can apply the voltage divider rule to the series circuit analyzed in the lab as follows:
Note that the voltage across the 1.5KΩ resistor is measured between the junction of the two resistors and the sero potential ground.
Parallel circuits are defined as circuits in which the same voltage appears across all elements. While all of the elements have the same voltage across them, the current flowing into a parallel circuit is divided among its parallel elements. For this reason, the parallel circuit is sometimes referred to as a current divider. We often need to know the current flowing through a particular circuit element, and this can be easily calculated using the current divider rule, which only requires knowledge of the circuit element values and the current flowing into the series circuit. There are at least two forms of the current divider rule that are in common use, and we will use the one that has the same form as the voltage divider rule, but with conductances replacing resistances, as this form is easy to remember once the voltage divider rule has been learned. We will use a resistive circuit to derive the current divider rule.
If we apply a current IT (T is for Total) across a parallel circuit comprised of resistors, as illustrated below, a voltage V is developed across the circuit. The current IT is the sum of the currents flowing in each resistor, and is calculated using Kirchhoff's current law as:
Now is a good time to introduce conductance, G, which is defined as the reciprocal of resistance, or G = 1/R. We can substitute G for 1/R in the above equation and rewrite it as:
The current Im flowing through a resistor Rm in the parallel circuit can be calculated using Ohm's law as:
If we substitute V from the first equation into the above equation, we can solve for Im as:
From this result, we can see that the current divider rule has the same form as the voltage divider rule, with IT substituted for VT and conductances substituted for resistances. The current divider rule for resistors shows that the current flowing through any resistor in a parallel connection is equal to the total current flowing into the parallel circuit multiplied by the ratio of the value of the conductance of interest to the sum of all of the conductances in the circuit. This ratio represents the percentage of the total current flowing into the parallel circuit that flows through the resistor of interest. We can apply the current divider rule to the parallel circuit analyzed in the lab as follows:
The rules can be extended to other…..