This is an old revision of the document!
VideoNumberHere
Common-emitter and emitter-follower amplifiers are the most widely used single-transistor amplifiers. The common-base configuration, illustrated below in its basic NPN form, is used less frequently as a stand-alone voltage amplifier stage, mostly because it has a low input resistance, but it is often combined with a common-emitter stage to form a cascode amplifier. In a common-base voltage amplifier, the input voltage is applied to the emitter and the output voltage is taken from the collector, and the input and output voltages are in-phase. The in-phase relationship can be understood by observing that when the signal voltage applied to the emitter increases, the base-emitter voltage vBE decreases, causing the emitter/collector current to decrease, decreasing the voltage drop across the collector resistor, RC, thereby increasing the collector voltage. Because of its low input resistance, the common-base amplifier is sometimes used as a current-in/voltage-out amplifier. Its operation in the cascode configuration is something like this because it takes the collector current from the common-emitter stage and produces an output voltage at its collector.
As with all linear Class A BJT amplifiers, the transistor must operate in the forward active region in the common-base amplifier. This means that the base-emitter junction must be forward biased, the collector-base junction must be reverse biased, and operation must be prevented from entering the saturation region. These bias conditions can be seen in the schematic shown in the “Procedure” section for the common-base stage as well as the CE stage in the cascode amplifier. The base is often biased using a resistive voltage divider, voltage regulator, or available power supply, and an emitter resistor, RE is used to establish the emitter current. The base should always be bypassed with a capacitor that produces a low impedance AC ground at all signal frequencies. If the amplifier is DC-coupled, the voltage source applied to the base must also provide a low DC resistance. The collector circuit is similar to what is used in the common-emitter amplifier, and in its simplest form consists of a resistor, RC connected between the collector and the power supply.
The input of a common-base amplifier looks into the emitter, which is the same as looking into the output resistance of an emitter-follower amplifier. As we saw in the “Class A NPN Emitter-Follower Amplifier” lab, the emitter-follower output resistance is low, which is desirable for a voltage amplifier output, but is not desirable for a voltage amplifier input. With a low-impedance voltage source providing the base bias, the common-base input resistance is simply re, which is equal to the ratio of the thermal voltage VT to the collector bias current IC, or RIN = VT/IC ≈ 26 mV/IC at room temperature. The gain of a common-base amplifier can be calculated using detailed circuit analysis or approximated by inspection as was done with the CE amplifier. Using the same approach as was done with the CE amplifier, the gain of the common-base amplifier with a low-impedance base driving circuit is AV = RC/re. Besides the low input resistance issue, the gain of the common-base amplifier depends on re, which is small (producing high gain, which may not be desirable), temperature dependent, and nonlinear. When combined with a CE stage to form a cascode amplifier, we will see that the re of the common-base amplifier becomes the effective collector resistance of the CE stage, and gets cancelled out of the cascode amplifier gain equation when the emitter resistor is 100% capacitively bypassed. The greatest advantage of the cascode amplifier, however, is that it reduces the Miller effect, which causes the bandwidth of a CE stage to decrease as its gain increases. With the re of the common-base stage as the effective collector resistance of the CE stage and the re of the CE stage as the emitter resistance when the emitter bias-setting resistor is fully bypassed, the gain of the CE stage is -re/re ≈ -1 when the two transistors are well-matched. The voltage gain is provided by the collector current flowing through the collector resistor in the common-base stage, and the common-base amplifier bandwidth is not diminished by the Miller effect. The important benefit realized by the cascode configuration is that high gains can be achieved without significant bandwidth loss due to the Miller effect, but it requires two transistors. As with CE amplifiers, an emitter-follower stage is often added on the output of the common-base stage to drive low impedance loads.
In this lab, we will not build a standalone common-base amplifier, but will instead study the use of the common-base amplifier in a cascode amplifier.
To understand the operating principles of common-base and cascode amplifiers. To design, build, and test a cascode amplifier using two 2N3904 NPN transistor stages, with an input resistance of at least 1 KΩ and a voltage gain of a little less than 10. To understand how to set up the proper bias conditions for a cascode amplifier and verify that the bias voltages in the circuit are close to their designed values. Following completion of this lab you should be able to explain the basic operation of common-base and cascode amplifiers, and be able to calculate the voltage gain for each of these amplifiers.
The emitter-follower amplifier presents a high input resistance to signals applied to its base and provides a low resistance effective voltage source at its output. These characteristics make the emitter-follower amplifier well suited for use as a voltage buffer amplifier. Buffer amplifiers are used to buffer heavy loads from signal sources that have a high output resistance. A good buffer has a high input resistance so as not to significantly load the output resistance of the source that is being buffered and a low resistance voltage source output that is capable of driving heavy loads with minimal loading loss.
Our amplifier needs to drive a 47 Ω load with a +/-1 V sine wave, which requires approximately +/-21 mA. We will make the base bias point at about mid-supply. Starting with a mid-supply base bias voltage, we can estimate the emitter voltage to be 2.5 V - 0.7 V = 1.8 V. We have a 68 Ω resistor in the kit, and if we use this for our RE, we get an emitter current of 1.8 V/68 Ω ≈ 26.5 mA. This exceeds our minimum current of 21 mA, so we will start with this. If we want to make a first-round estimate of the voltage drop incurred due to base current, remembering that iE ≈ iC, we use β = 200 to estimate the base current as iB ≈ 26.5 mA/200 ≈ 133 μA. The base bias current is on the high side because we are using a large emitter current. The voltage drop due to the base current can be estimated to be (133 μA)(2.2 KΩ||2.2 KΩ) ≈ 0.15 V. This reduction will in turn reduce the emitter voltage, which will reduce the emitter current, which will reduce the base current and its associated voltage drop, so a reasonable estimate for base bias voltage reduction due to base bias current would be about 0.1 V, so we will use 2.4 V for the base voltage. Now, a more accurate emitter bias voltage can be established as 2.4 V - 0.7 V = 1.7 V. The emitter bias current can be calculated as 1.7 V/68 Ω = 25 mA.
The input resistance looking into the base of the transistor used in the emitter-follower amplifier Ri,base is the same as that of the CE amplifier
Using β = 200 from the Introduction to Transistors lab, and substituting numbers from this lab, we have
When we use the voltage divider to provide base bias, we need to include the resistors in the divider in parallel with the input resistance looking into the base, so the total input resistance Riis
Note that this result falls slightly short of our design goal of having a minimum input resistance of 1 KΩ. This is primarily due to the 2.2 KΩ resistors that were used to set up the base bias voltage. We could increase the value of these resistors a small amount and raise the input resistance to at least 1 KΩ, but the next largest value in the kit is 4.7 KΩ, which would give us considerably more unnecessary voltage drop on the base bias voltage. The best solution, if all commercially available resistor values were available, would be to use the smallest available resistor value that meets the input resistance requirement.
For large β (≥ 100) the output resistance looking into the emitter of the emitter-follower amplifier Ro is calculated as
where RS is the total equivalent source resistance in the base circuit. In our circuit, RS is equal to the parallel combination of the base bias resistors and the source resistance feeding the base. Note that when the emitter-follower amplifier is fed by the low resistance voltage source output of the M1K, RS ≈ 0 and the output resistance is simply the incremental emitter resistance re.
When we place the emitter-follower on the output of the CE amplifier from the “Class A NPN Common-Emitter Amplifier” lab, we have nonzero RS, and need to include it in out calculation of Ro
We will see a small voltage divider loss when driving the 47 Ω load, and a more pronounced loss when driving the 10 Ω load. With the emitter-follower amplifier buffering the CE amplifier, we will have voltage divider factors of 47 Ω/49.6 Ω ≈ 0.95 for the 47 Ω load and 10 Ω/12.6 Ω ≈ 0.79 for the 10 Ω load.
We can calculate the efficiency of the emitter-follower amplifier studied in this lab.
For the emitter-follower amplifier by itself driving +/-1 V into the 47 Ω load resistor, the power into the load is:
Note that the power into the load could also have been calculated using the [vLOAD(rms)]2/RL formula.
The quiescent power drawn from the supply is:
The efficiency is therefore:
For the emitter-follower amplifier buffering the CE amplifier driving +/-1 V into the 47 Ω load resistor, the power into the load is again:
The total quiescent power drawn from the supply, using the results already calculated in the CE amplifier lab, is:
The efficiency is therefore:
If we substitute the 10 Ω load for the 47 Ω load, we can only deliver about +/- 0.25 V to the load, and the power into the load is
The efficiency is now only
It is important to note that the voltage divider losses between the emitter-follower output and the load were omitted.
We can calculate the power gain of the two cascaded amplifiers with the 47 Ω load using the results obtained in the “Class A NPN Common-Emitter Amplifier” lab. The voltage gain is essentially the same as it was for the CE amplifier because the voltage gain of the emitter-follower amplifier is very close to unity and the input resistance of the CE is unchanged. The power gain is therefore
From this result, we can see how adding the emitter-follower output stage increased the overall power gain by providing current gain to drive the heavier load.