Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:courses:engineering_discovery:lab_11 [19 Oct 2016 21:20] Jonathan Pearsonuniversity:courses:engineering_discovery:lab_11 [03 Jan 2018 19:38] (current) – [Observations and Conclusions] Doug Mercer
Line 1: Line 1:
 ===== Class A NPN Emitter-Follower Amplifier ===== ===== Class A NPN Emitter-Follower Amplifier =====
-{{ analogTV>VideoNumberHere}} +{{ analogTV>5180379850001}}
  
 ==== Introduction ==== ==== Introduction ====
-The common-emitter amplifier introduced in the "Class A NPN Common-Emitter Amplifier" lab provided voltage and current amplification, but suffered from a large output resistance that was equal to the equivalent collector resistance that was present for AC signals.  The emitter-follower, EF, also called common-collector, CC, amplifier provides nearly unity voltage gain and current gain, which can be large, and low output resistance.  Emitter-follower amplifiers are commonly used as output stages that are capable of driving low impedance loads due to their current gains and low output resistances.  The name "emitter-follower" originates from the fact that the output signal, taken at the emitter, follows the input signal, applied at the base, with nearly unity gain.  "Emitter-follower" is more descriptive than "common-collector," and will be used henceforth for this reason.  As with the CE amplifier, we will study the EF amplifier using a single transistor biased in a Class A configuration.+The common-emitter amplifier introduced in the "Class A NPN Common-Emitter Amplifier" lab provided voltage and current amplification, but suffered from a large output resistance that was equal to the equivalent collector resistance that was present for AC signals.  The emitter-follower, EF, also called common-collector, CC, amplifier provides nearly unity voltage gainand current gain, which can be large, and low output resistance.  Emitter-follower amplifiers are commonly used as output stages that are capable of driving low impedance loads due to their current gains and low output resistances.  The name "emitter-follower" originates from the fact that the output signal, taken at the emitter, follows the input signal, applied at the base, with nearly unity gain.  "Emitter-follower" is more descriptive than "common-collector," and will be used henceforth for this reason.  As with the CE amplifier, we will study the EF amplifier using a single transistor biased in a Class A configuration.
  
 Unlike the CE amplifier, the output voltage and input voltage of an EF amplifier are in-phase with each other and of nearly the same magnitude.  This is the sense in which the output voltage at the emitter "follows" the input.  The collector is generally connected directly to the power supply and the emitter is connected to another supply voltage -- often ground -- through an emitter resistor, R<sub>E</sub> The operation of an EF amplifier constitutes a form of negative feedback.  Negative feedback systems are discussed in further detail in later labs, but can be briefly described as systems in which part or all of an output quantity is fed back upstream in the system in such a way as to reduce an error that exists between the existing condition and the desired condition.  Automotive cruise control is an example of an everyday negative feedback system in which the speed of an automobile is constantly monitored and adjusted in such a way as to minimize the error between the current speed and the speed set by the driver.  Negative feedback systems are often used to regulate physical phenomena.  Reference to the schematic in the Procedure section of the lab will be helpful when reading the remainder of this section.  In the emitter-follower amplifier, the negative feedback occurs as follows: starting at the emitter, as the emitter voltage v<sub>E</sub> increases, the base-emitter voltage v<sub>BE</sub> decreases, which in turn reduces the base current i<sub>B</sub>, which reduces the collector current i<sub>C</sub> by the i<sub>C</sub> = βi<sub>B</sub> relationship; recalling that for large β we can say that i<sub>E</sub> ≈ i<sub>C</sub> (the exact relationship between i<sub>E</sub> and i<sub>B</sub>) is i<sub>E</sub> = (1 + β)i<sub>B</sub>, and (1 + β)i<sub>B</sub> ≈ βi<sub>B</sub> for large β) we see that i<sub>E</sub> decreases as i<sub>C</sub>, thuis reducing v<sub>E</sub>  This negative feedback action regulates the bias point and voltage gain of the emitter-follower, keeping the voltage gain close to unity.  This same feedback loop helps regulate the operating bias point in the CE amplifier.  In many, if not most, applications, we can view the emitter follower as having unity voltage gain with the output voltage shifted down from the input voltage by one v<sub>BE</sub> drop.  The bias point considerations for the Class A emitter-follower amplifier are the same as for the Class A CE amplifier. Unlike the CE amplifier, the output voltage and input voltage of an EF amplifier are in-phase with each other and of nearly the same magnitude.  This is the sense in which the output voltage at the emitter "follows" the input.  The collector is generally connected directly to the power supply and the emitter is connected to another supply voltage -- often ground -- through an emitter resistor, R<sub>E</sub> The operation of an EF amplifier constitutes a form of negative feedback.  Negative feedback systems are discussed in further detail in later labs, but can be briefly described as systems in which part or all of an output quantity is fed back upstream in the system in such a way as to reduce an error that exists between the existing condition and the desired condition.  Automotive cruise control is an example of an everyday negative feedback system in which the speed of an automobile is constantly monitored and adjusted in such a way as to minimize the error between the current speed and the speed set by the driver.  Negative feedback systems are often used to regulate physical phenomena.  Reference to the schematic in the Procedure section of the lab will be helpful when reading the remainder of this section.  In the emitter-follower amplifier, the negative feedback occurs as follows: starting at the emitter, as the emitter voltage v<sub>E</sub> increases, the base-emitter voltage v<sub>BE</sub> decreases, which in turn reduces the base current i<sub>B</sub>, which reduces the collector current i<sub>C</sub> by the i<sub>C</sub> = βi<sub>B</sub> relationship; recalling that for large β we can say that i<sub>E</sub> ≈ i<sub>C</sub> (the exact relationship between i<sub>E</sub> and i<sub>B</sub>) is i<sub>E</sub> = (1 + β)i<sub>B</sub>, and (1 + β)i<sub>B</sub> ≈ βi<sub>B</sub> for large β) we see that i<sub>E</sub> decreases as i<sub>C</sub>, thuis reducing v<sub>E</sub>  This negative feedback action regulates the bias point and voltage gain of the emitter-follower, keeping the voltage gain close to unity.  This same feedback loop helps regulate the operating bias point in the CE amplifier.  In many, if not most, applications, we can view the emitter follower as having unity voltage gain with the output voltage shifted down from the input voltage by one v<sub>BE</sub> drop.  The bias point considerations for the Class A emitter-follower amplifier are the same as for the Class A CE amplifier.
Line 47: Line 46:
   - Calculate the rms power dissipation in the load resistor   - Calculate the rms power dissipation in the load resistor
   - Estimate the voltage swing that would be present across the 47 Ω load resistor if it were driven by the CE stage alone, without the emitter-follower buffer in place   - Estimate the voltage swing that would be present across the 47 Ω load resistor if it were driven by the CE stage alone, without the emitter-follower buffer in place
-  - Reduce the swing of the input voltage to 2.493 V to 2.507 V+  - Reduce the swing of the input voltage to 2.48 V to 2.52 V
   - Replace the 47 Ω load resistor with a 10 Ω resistor    - Replace the 47 Ω load resistor with a 10 Ω resistor 
-  - Verify that the output voltage swings 250 mV<sub>P-P</sub> about the 2.5 V bias voltage+  - Verify that the output voltage swings 300 mV<sub>P-P</sub> about the 2.5 V bias voltage
   - Calculate the load current into the 10 Ω load resistor   - Calculate the load current into the 10 Ω load resistor
 ==== Theory ==== ==== Theory ====
 The emitter-follower amplifier presents a high input resistance to signals applied to its base and provides a low resistance effective voltage source at its output.   These characteristics make the emitter-follower amplifier well suited for use as a voltage //buffer// amplifier.  Buffer amplifiers are used to buffer heavy loads from signal sources that have a high output resistance.  A good buffer has a high input resistance so as not to significantly load the output resistance of the source that is being buffered and a low resistance voltage source output that is capable of driving heavy loads with minimal loading loss. The emitter-follower amplifier presents a high input resistance to signals applied to its base and provides a low resistance effective voltage source at its output.   These characteristics make the emitter-follower amplifier well suited for use as a voltage //buffer// amplifier.  Buffer amplifiers are used to buffer heavy loads from signal sources that have a high output resistance.  A good buffer has a high input resistance so as not to significantly load the output resistance of the source that is being buffered and a low resistance voltage source output that is capable of driving heavy loads with minimal loading loss.
  
-Our amplifier needs to drive a 47 Ω load with a +/-V sine wave, which requires approximately +/-21 mA.  We will make the base bias point at about mid-supply.  Starting with a mid-supply base bias voltage, we can estimate the emitter voltage to be 2.5 V - 0.7 V = 1.8 V.  We have 68 Ω resistor in the kit, and if we use this for our R<sub>E</sub>, we get an emitter current of 1.8 V/68 Ω ≈ 26.5 mA.  This exceeds our minimum current of 21 mA, so we will start with this.  If we want to make a first-round estimate of the voltage drop incurred due to base current, remembering that i<sub>E</sub> ≈ i<sub>C</sub>, we use β = 200 to estimate the base current as i<sub>B</sub> ≈ 26.5 mA/200 ≈ 133 μA.  The base bias current is on the high side because we are using a large emitter current.  The voltage drop due to the base current can be estimated to be (133 μA)(2.2 KΩ||2.2 KΩ) ≈ 0.15 V.  This reduction will in turn reduce the emitter voltage, which will reduce the emitter current, which will reduce the base current and its associated voltage drop, so a reasonable estimate for base bias voltage reduction due to base bias current would be about 0.1 V, so we will use 2.4 V for the base voltage.  Now, a more accurate emitter bias voltage can be established as 2.4 V - 0.7 V = 1.7 V.  The emitter bias current can be calculated as 1.7 V/68 Ω = 25 mA.+Our amplifier needs to drive a 47 Ω load with a +/-0.5 V sine wave, which requires approximately +/-10.6 mA.  We will make the base bias point at about mid-supply.  Starting with a mid-supply base bias voltage, we can estimate the emitter voltage to be 2.5 V - 0.7 V = 1.8 V.  When the output sine wave is at its minimum level, the emitter resistor must sink all of the current fed back from the load (remember that the 47 μF capacitor acts like short circuit to the 500 Hz signal compared with the 47 Ω load resistor).  The current from the emitter backs offallowing the current flowing back from the load to pass through the emitter resistor.  A KCL calculation made at the emitter shows that the current out of the emitter is equal to the sum of the current flowing to ground through the emitter resistor and the current fed back from the load.  The current flowing through the emitter resistor must therefore be at least equal to the maximum current flowing back from the load when the output waveform is at its minimumotherwise we would have to have a negative emitter current.  When the output signal is at its minimum, the voltage on the emitter is approximately 1.8 V - 0.5 V = 1.3 V.  The maximum current flowing back from the load, which occurs at the waveform minimum, was determined to be 10.6 mA.  The emitter current must be at least this large at this point so the maximum emitter resistor value is 1.3 V/10.6 mA ≈ 123 Ω.  We want to have some margin, and 100 Ω would be a little too close, so we will go with the next smallest value of 68 Ω for the emitter resistor.  This value gives an approximate Q-point bias current of 1.8 V/68 Ω ≈ 26.5 mA. 
 + 
 +If we want to make a first-round estimate of the voltage drop incurred due to base current, remembering that i<sub>E</sub> ≈ i<sub>C</sub>, we use β = 200 to estimate the base current as i<sub>B</sub> ≈ 26.5 mA/200 ≈ 133 μA.  The base bias current is on the high side because we are using a large emitter current.  The voltage drop due to the base current can be estimated to be (133 μA)(2.2 KΩ||2.2 KΩ) ≈ 0.15 V.  This reduction will in turn reduce the emitter voltage, which will reduce the emitter current, which will reduce the base current and its associated voltage drop, so a reasonable estimate for base bias voltage reduction due to base bias current would be about 0.1 V, so we will use 2.4 V for the base voltage.  Now, a more accurate emitter bias voltage can be established as 2.4 V - 0.7 V = 1.7 V.  The emitter bias current can be calculated as 1.7 V/68 Ω = 25 mA.
  
 The input resistance looking into the base of the transistor used in the emitter-follower amplifier R<sub>i,base</sub> is the same as that of the CE amplifier The input resistance looking into the base of the transistor used in the emitter-follower amplifier R<sub>i,base</sub> is the same as that of the CE amplifier
Line 88: Line 89:
 For the emitter-follower amplifier by itself driving +/-1 V into the 47 Ω load resistor, the power into the load is: For the emitter-follower amplifier by itself driving +/-1 V into the 47 Ω load resistor, the power into the load is:
  
-<m>P_LOAD = (1/√2)({V_PEAK})(1/√2)({21.mA_PEAK}) = 10.mW_rms</m>+<m>P_LOAD = (1/√2)({0.5 V_PEAK})(1/√2)({10.mA_PEAK}) = 2.65 mW_rms</m>
  
 Note that the power into the load could also have been calculated using the [v<sub>LOAD</sub>(rms)]<sup>2</sup>/R<sub>L</sub> formula. Note that the power into the load could also have been calculated using the [v<sub>LOAD</sub>(rms)]<sup>2</sup>/R<sub>L</sub> formula.
Line 98: Line 99:
 The efficiency is therefore: The efficiency is therefore:
  
-<m>eta = {10.mW}/{82.5 mW} ≈ 12.8%</m>+<m>eta = {2.65 mW}/{82.5 mW} ≈ 3.2%</m>
  
-For the emitter-follower amplifier buffering the CE amplifier driving +/-V into the 47 Ω load resistor, the power into the load is again:+For the emitter-follower amplifier buffering the CE amplifier driving +/-0.5 V into the 47 Ω load resistor, the power into the load is again:
  
-<m>P_LOAD = 10.mW_rms</m>+<m>P_LOAD = 2.65 mW_rms</m>
  
 The total quiescent power drawn from the supply, using the results already calculated in the CE amplifier lab, is: The total quiescent power drawn from the supply, using the results already calculated in the CE amplifier lab, is:
Line 110: Line 111:
 The efficiency is therefore: The efficiency is therefore:
  
-<m>eta = {10.mW}/{102 mW} ≈ 10.4%</m>+<m>eta = {2.65 mW}/{102 mW} ≈ 2.6%</m>
  
-If we substitute the 10 Ω load for the 47 Ω load, we can only deliver about +/- 0.25 to the load, and the power into the load is+If we substitute the 10 Ω load for the 47 Ω load, we lower the output voltage across the load to about +/- 0.15 V, and the power into the load is
  
-<m>P_LOAD = (1/√2)({0.25 V_PEAK})(1/√2)({25 mA_PEAK}) = 3.mW_rms</m>+<m>P_LOAD = (1/√2)({0.15 V_PEAK})(1/√2)({12.5 mA_PEAK}) = 0.94 mW_rms</m>
  
 The efficiency is now only The efficiency is now only
  
-<m>eta = {3.mW}/{102 mW} ≈ 3.0%</m>+<m>eta = {0.94 mW}/{102 mW} ≈ 0.92%</m>
  
 It is important to note that the voltage divider losses between the emitter-follower output and the load were omitted. It is important to note that the voltage divider losses between the emitter-follower output and the load were omitted.
Line 135: Line 136:
   * Emitter-follower amplifiers are often used to buffer heavy loads that require large output currents from sources that have high source resistances   * Emitter-follower amplifiers are often used to buffer heavy loads that require large output currents from sources that have high source resistances
   * Adding an emitter-follower stage to a CE amplifier can significantly increase the power gain of the overall amplifier   * Adding an emitter-follower stage to a CE amplifier can significantly increase the power gain of the overall amplifier
 +
 +**Return to [[university:courses:engineering_discovery|Engineering Discovery Index]]**
university/courses/engineering_discovery/lab_11.txt · Last modified: 03 Jan 2018 19:38 by Doug Mercer