Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:courses:electronics:text:chapter-9 [06 Jun 2017 17:19] – [9.2.5 common emitter and source Lab Activities] Doug Mercer | university:courses:electronics:text:chapter-9 [07 Oct 2020 16:34] – [AT2 Bootstrapping for Higher Input Impedance] Doug Mercer |
---|
Again looking at the small signal models in figure 9.3.1 we see that for both the BJT case and the MOS case the output impedance is the parallel combination of R<sub>L</sub> and r<sub>o</sub>. We can generally assume this is true if we consider that V<sub>in</sub> is driven from a low impedance (nearly ideal) voltage source. If this is not the case then the finite output impedance must be added in series with r<sub>o</sub>. If the input of the current follower is driven by the relatively high output impedance of a transconductance amplifier such as the common emitter or source amplifier from earlier then the output impedance for the combined amplifier can be very high. For most practical applications we can ignore r<sub>o</sub> because it is very often much larger than R<sub>L</sub>. | Again looking at the small signal models in figure 9.3.1 we see that for both the BJT case and the MOS case the output impedance is the parallel combination of R<sub>L</sub> and r<sub>o</sub>. We can generally assume this is true if we consider that V<sub>in</sub> is driven from a low impedance (nearly ideal) voltage source. If this is not the case then the finite output impedance must be added in series with r<sub>o</sub>. If the input of the current follower is driven by the relatively high output impedance of a transconductance amplifier such as the common emitter or source amplifier from earlier then the output impedance for the combined amplifier can be very high. For most practical applications we can ignore r<sub>o</sub> because it is very often much larger than R<sub>L</sub>. |
| |
| **ADALM1000 Lab Activity, [[university:courses:alm1k:alm-lab-cb|BJT Common Base Amplifier]]**\\ |
| **ADALM1000 Lab Activity, [[university:courses:alm1k:alm-lab-cg|BJT Common Gate Amplifier]]**\\ |
| **ADALM1000 Lab Activity, [[university:courses:alm1k:alm-lab-fca|Folded Cascode Amplifier]]** |
==== 9.4 Voltage followers (also called Emitter or Source follower or Common collector or drain amplifiers) ==== | ==== 9.4 Voltage followers (also called Emitter or Source follower or Common collector or drain amplifiers) ==== |
| |
====9.4.5 Voltage Follower (common collector or drain) Lab Activities ==== | ====9.4.5 Voltage Follower (common collector or drain) Lab Activities ==== |
| |
[[university:courses:electronics:electronics-lab-11|BJT Emitter follower]]\\ | **ADALM1000 Lab Activity 11, [[university:courses:alm1k:alm-lab-11|BJT Emitter follower]]**\\ |
[[university:courses:electronics:electronics-lab-11m|MOS source follower]]\\ | **ADALM1000 Lab Activity 11M, [[university:courses:alm1k:alm-lab-11m|MOS Source follower]]** |
| |
| **ADALM2000 Lab Activity 11, [[university:courses:electronics:electronics-lab-11|BJT Emitter follower]]**\\ |
| **ADALM2000 Lab Activity 11m, [[university:courses:electronics:electronics-lab-11m|MOS Source follower]]** |
| |
=====9.5 Series Feedback: emitter/source degeneration===== | =====9.5 Series Feedback: emitter/source degeneration===== |
The impedance R<sub>E</sub> reduces the overall transconductance g<sub>m</sub> of the circuit by a factor of g<sub>m</sub>R<sub>E</sub> + 1, which makes the voltage gain: | The impedance R<sub>E</sub> reduces the overall transconductance g<sub>m</sub> of the circuit by a factor of g<sub>m</sub>R<sub>E</sub> + 1, which makes the voltage gain: |
| |
| {{ :university:courses:electronics:text:chptr9-e17.png?290 |}} |
{{ :university:courses:electronics:text:chptr9-e17.png?300 |}} | |
(when g<sub>m</sub>R<sub>E</sub> >> 1) | (when g<sub>m</sub>R<sub>E</sub> >> 1) |
| |
Going back to our earlier biasing example, figure 9.5.1, values for I<sub>C</sub> = 2mA, R<sub>L</sub> = 3.4KΩ and R<sub>E</sub> = 3KΩ to calculate the small signal gain we first find g<sub>m</sub> = I<sub>C</sub>/V<sub>T</sub> = 2mA/25mV = 0.08. Using our formula for A<sub>V</sub>: | Going back to our earlier biasing example, figure 9.5.1, values for I<sub>C</sub> = 2mA, R<sub>L</sub> = 3.4KΩ and R<sub>E</sub> = 3KΩ to calculate the small signal gain we first find g<sub>m</sub> = I<sub>C</sub>/V<sub>T</sub> = 2mA/25mV = 0.08. Using our formula for A<sub>V</sub>: |
| |
{{ :university:courses:electronics:text:chptr9-e18.png?400 |}} | {{ :university:courses:electronics:text:chptr9-e18.png?300 |}} |
| |
====9.5.2 Small signal input impedance with emitter/source degeneration==== | ====9.5.2 Small signal input impedance with emitter/source degeneration==== |
Again looking at the small signal models in figure 9.4.1 we see that for the BJT case the input V<sub>in</sub> see r<sub></sub>in series with degeneration resistor R<sub>E</sub> as a load. For the MOS case V<sub>in</sub> see basically an open circuit. | Again looking at the small signal models in figure 9.4.1 we see that for the BJT case the input V<sub>in</sub> see r<sub></sub>in series with degeneration resistor R<sub>E</sub> as a load. For the MOS case V<sub>in</sub> see basically an open circuit. |
| |
{{ :university:courses:electronics:text:chptr9-e21.png?200 |}} | {{ :university:courses:electronics:text:chptr9-e19.png?200 |}} |
| |
====9.5.3 Small signal output impedance with emitter/source degeneration==== | ====9.5.3 Small signal output impedance with emitter/source degeneration==== |
Using our earlier biasing exercise in figure 9.5.1 as an example but splitting the 3KΩ R<sub>E</sub> into two resistors as in figure 9.5.4 with R<sub>E1</sub>= 1KΩ and R<sub>E2</sub> = 2KΩ with C<sub>1</sub> = 1uF we can recalculate the small signal gain for high frequencies, where C<sub>1</sub> effectively shorts out R<sub>E2</sub>, to be: | Using our earlier biasing exercise in figure 9.5.1 as an example but splitting the 3KΩ R<sub>E</sub> into two resistors as in figure 9.5.4 with R<sub>E1</sub>= 1KΩ and R<sub>E2</sub> = 2KΩ with C<sub>1</sub> = 1uF we can recalculate the small signal gain for high frequencies, where C<sub>1</sub> effectively shorts out R<sub>E2</sub>, to be: |
| |
{{ :university:courses:electronics:text:chptr9-e22.png?200 |}} | {{ :university:courses:electronics:text:chptr9-e20.png?300 |}} |
| |
The addition of by-pass capacitor C<sub>1</sub>, however, modifies the low frequency response of the circuit. We know from our two gain calculations that the DC gain of the circuit is -1.13 and the gain increases to -3.36 for high frequencies. We can therefore assume that the frequency response consists of a relatively low frequency zero followed by a somewhat higher frequency pole. The formulas for the zero and pole are as follows: | The addition of by-pass capacitor C<sub>1</sub>, however, modifies the low frequency response of the circuit. We know from our two gain calculations that the DC gain of the circuit is -1.13 and the gain increases to -3.36 for high frequencies. We can therefore assume that the frequency response consists of a relatively low frequency zero followed by a somewhat higher frequency pole. The formulas for the zero and pole are as follows: |
| |
<m> F_Z = 1/(2πR_E2 C_1) </m> | <m>F_Z = 1/(2 pi R_E2 C_1)</m> |
| |
<m> F_P = 1/(2R'_E C_1) </m> | <m>F_P = 1/(2R prime _E C_1)</m> |
| |
where R’<sub>E</sub>= R<sub>E2</sub> || (R<sub>E1</sub> + r<sub>e</sub>) | where R’<sub>E</sub>= R<sub>E2</sub> || (R<sub>E1</sub> + r<sub>e</sub>) |
| |
<m> I_b = (V_+ - V_BE ) / (R_F + (β + 1 )R_L ) </m> | <m> I_b = (V_+ - V_BE ) / (R_F + (β + 1 )R_L ) </m> |
| |
{{ :university:courses:electronics:text:chptr9-e23.png?200 |}} | |
| |
If V<sub>BE</sub> is held constant and temperature increases, then the collector current I<sub>c</sub> increases. However, a larger I<sub>c</sub> causes the voltage drop across resistor R<sub>L</sub> to increase, which in turn reduces the voltage V<sub>RF</sub> across the base resistor R<sub>F</sub>. A lower base-resistor voltage drop reduces the base current I<sub>b</sub>, which results in less collector current I<sub>c</sub>. Because an increase in collector current with temperature is opposed, the operating point is kept more stable. | If V<sub>BE</sub> is held constant and temperature increases, then the collector current I<sub>c</sub> increases. However, a larger I<sub>c</sub> causes the voltage drop across resistor R<sub>L</sub> to increase, which in turn reduces the voltage V<sub>RF</sub> across the base resistor R<sub>F</sub>. A lower base-resistor voltage drop reduces the base current I<sub>b</sub>, which results in less collector current I<sub>c</sub>. Because an increase in collector current with temperature is opposed, the operating point is kept more stable. |
<WRAP centeralign > Figure AT1.2 Inserting R<sub>2</sub>increases the input resistance </WRAP> | <WRAP centeralign > Figure AT1.2 Inserting R<sub>2</sub>increases the input resistance </WRAP> |
| |
| <hidden> |
====AT2 Bootstrapping for Higher Input Impedance==== | ====AT2 Bootstrapping for Higher Input Impedance==== |
| |
| |
Otherwise, components can be chosen exactly as before. The bootstrapping capacitor C<sub>B</sub> must be very large so that it looks like a short circuit to signal frequencies. Theoretically, the resistor R<sub>B</sub> can be chosen arbitrarily. As long as Equation (A.1) can be met, a high choice of R<sub>B</sub> (e.g., R<sub>B</sub> > 1 kΩ) is a good idea. The signal at the transistor’s emitter follows the signal at its base. At signal frequencies, C<sub>B</sub> acts like a short circuit, and so both ends of R<sub>B</sub> see the same potential. Hence, R<sub>B</sub> carries no current at signal frequencies. Thus, the R1–R2 divider cannot load the input source because no current from the source makes its way across R<sub>B</sub> (i.e., R<sub>B</sub> ≈ ∞ at signal frequencies). The current through R1–R2 that would normally come from the source comes from the output instead. This method is called bootstrapping because we use the circuit’s own output to reduce current required from the input. | Otherwise, components can be chosen exactly as before. The bootstrapping capacitor C<sub>B</sub> must be very large so that it looks like a short circuit to signal frequencies. Theoretically, the resistor R<sub>B</sub> can be chosen arbitrarily. As long as Equation (A.1) can be met, a high choice of R<sub>B</sub> (e.g., R<sub>B</sub> > 1 kΩ) is a good idea. The signal at the transistor’s emitter follows the signal at its base. At signal frequencies, C<sub>B</sub> acts like a short circuit, and so both ends of R<sub>B</sub> see the same potential. Hence, R<sub>B</sub> carries no current at signal frequencies. Thus, the R1–R2 divider cannot load the input source because no current from the source makes its way across R<sub>B</sub> (i.e., R<sub>B</sub> ≈ ∞ at signal frequencies). The current through R1–R2 that would normally come from the source comes from the output instead. This method is called bootstrapping because we use the circuit’s own output to reduce current required from the input. |
| </hidden> |
| |
**Return to [[university:courses:electronics:text:chapter-8|Previous Chapter]]** | **Return to [[university:courses:electronics:text:chapter-8|Previous Chapter]]** |