This shows you the differences between two versions of the page.
Next revisionBoth sides next revision | |||
university:courses:electronics:text:chapter-4 [30 Aug 2013 17:04] – created Doug Mercer | university:courses:electronics:text:chapter-4 [30 Aug 2013 17:07] – [4.9 Operational amplifier Schmitt trigger] Doug Mercer | ||
---|---|---|---|
Line 218: | Line 218: | ||
The fact that the positive feedback applied within the circuit ensures that there is effectively a higher gain and therefore the switching is faster. This is particularly useful when the input waveform may be slow. However a speed up capacitor can be applied within the Schmitt trigger circuit to increase the switching speed still further. By placing a capacitor across the positive feedback resistor R< | The fact that the positive feedback applied within the circuit ensures that there is effectively a higher gain and therefore the switching is faster. This is particularly useful when the input waveform may be slow. However a speed up capacitor can be applied within the Schmitt trigger circuit to increase the switching speed still further. By placing a capacitor across the positive feedback resistor R< | ||
+ | |||
+ | **Return to [[university: | ||
+ | |||
+ | **Go to Next Chapter** | ||
+ | |||
+ | **Return to [[university: | ||