This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:text:chapter-1 [28 Aug 2013 17:13] – [Section Review:] Doug Mercer | university:courses:electronics:text:chapter-1 [05 Jun 2017 15:48] (current) – [1.5 Review of Thévenin's theorem] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======1: | + | ======Chapter |
This introductory chapter will serve as a quick review of a few of the more important topics from the earlier courses Circuits I and II. It can be skipped if the reader feels he or she is sufficiently familiar with these fundamental circuit analysis and design concepts. | This introductory chapter will serve as a quick review of a few of the more important topics from the earlier courses Circuits I and II. It can be skipped if the reader feels he or she is sufficiently familiar with these fundamental circuit analysis and design concepts. | ||
Line 75: | Line 75: | ||
A matrix version of Kirchhoff' | A matrix version of Kirchhoff' | ||
+ | [[university: | ||
====1.4.2 Kirchhoff' | ====1.4.2 Kirchhoff' | ||
Line 123: | Line 124: | ||
Figure 1.5.1 Any black box containing only voltage sources, current sources, and other resistors can be converted to a Thévenin equivalent circuit, comprising exactly one voltage source and one resistor. | Figure 1.5.1 Any black box containing only voltage sources, current sources, and other resistors can be converted to a Thévenin equivalent circuit, comprising exactly one voltage source and one resistor. | ||
- | **Review Lab Activity: [[university: | + | **Review Lab Activity: [[university: |
- | ]]** | + | **Review Lab Activity: [[university: |
=====1.6 Review of Norton' | =====1.6 Review of Norton' | ||
Line 133: | Line 134: | ||
Figure 1.6.1 Any black box containing only voltage sources, current sources, and resistors can be converted to a Norton equivalent circuit. | Figure 1.6.1 Any black box containing only voltage sources, current sources, and resistors can be converted to a Norton equivalent circuit. | ||
+ | |||
+ | [[university: | ||
=====1.7 Review of the Superposition Theorem===== | =====1.7 Review of the Superposition Theorem===== | ||
Line 212: | Line 215: | ||
The Superposition Theorem finds use in the study of alternating current (AC) circuits, and semiconductor (amplifier) circuits, where sometimes AC is often mixed (superimposed) with DC. Because AC voltage and current equations (Ohm's Law) are linear just like DC, we can use Superposition to analyze the circuit with just the DC power source, then just the AC power source, combining the results to tell what will happen with both AC and DC sources in effect. For now, though, Superposition will suffice as a break from having to do simultaneous equations to analyze a circuit. | The Superposition Theorem finds use in the study of alternating current (AC) circuits, and semiconductor (amplifier) circuits, where sometimes AC is often mixed (superimposed) with DC. Because AC voltage and current equations (Ohm's Law) are linear just like DC, we can use Superposition to analyze the circuit with just the DC power source, then just the AC power source, combining the results to tell what will happen with both AC and DC sources in effect. For now, though, Superposition will suffice as a break from having to do simultaneous equations to analyze a circuit. | ||
+ | [[university: | ||
====Section Review:==== | ====Section Review:==== | ||