This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
university:courses:electronics:text:chapter-10 [18 Nov 2015 03:16] – [10.2 Design Example] Doug Mercer | university:courses:electronics:text:chapter-10 [12 Aug 2021 00:30] (current) – The symbol for inf Loknath Bharti | ||
---|---|---|---|
Line 7: | Line 7: | ||
<WRAP centeralign > Figure 10.1 Two stage cascade amplifier </ | <WRAP centeralign > Figure 10.1 Two stage cascade amplifier </ | ||
- | It is necessary to consider what happens when non-ideal amplifiers are put in series. Looking at the example in figure 10.1, it is clear that the input and output resistances (or impedances) come into play by reducing the overall gain. If the amplifiers were ideal (R< | + | It is necessary to consider what happens when non-ideal amplifiers are put in series. Looking at the example in figure 10.1, it is clear that the input and output resistances (or impedances) come into play by reducing the overall gain. If the amplifiers were ideal (R< |
<WRAP indent > First amplification stage with loss between stage #1 and #2: </ | <WRAP indent > First amplification stage with loss between stage #1 and #2: </ |