This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
university:courses:electronics:text:chapter-10 [21 Sep 2013 16:59] – created Doug Mercer | university:courses:electronics:text:chapter-10 [12 Aug 2021 00:30] (current) – The symbol for inf Loknath Bharti | ||
---|---|---|---|
Line 7: | Line 7: | ||
<WRAP centeralign > Figure 10.1 Two stage cascade amplifier </ | <WRAP centeralign > Figure 10.1 Two stage cascade amplifier </ | ||
- | It is necessary to consider what happens when non-ideal amplifiers are put in series. Looking at the example in figure 10.1, it is clear that the input and output resistances (or impedances) come into play by reducing the overall gain. If the amplifiers were ideal (R< | + | It is necessary to consider what happens when non-ideal amplifiers are put in series. Looking at the example in figure 10.1, it is clear that the input and output resistances (or impedances) come into play by reducing the overall gain. If the amplifiers were ideal (R< |
<WRAP indent > First amplification stage with loss between stage #1 and #2: </ | <WRAP indent > First amplification stage with loss between stage #1 and #2: </ | ||
Line 102: | Line 102: | ||
In this respect consider further the implication that each stage gain depends largely on the ratio of the collector resistance to the (un bypassed) emitter resistance. | In this respect consider further the implication that each stage gain depends largely on the ratio of the collector resistance to the (un bypassed) emitter resistance. | ||
- | Respond critically | + | <note warning> |
- | + | ||
- | Similarly respond critically to the alternative suggestion of obtaining an order of magnitude increase in gain by decreasing the un bypassed emitter resistance by a factor of ten. | + | |
- | + | ||
- | {{ : | + | |
- | + | ||
- | <WRAP centeralign > Figure 10.2.2. Adding negative feedback </ | + | |
- | + | ||
- | {{ : | + | |
- | + | ||
- | <WRAP centeralign > Figure 10.2.3. </WRAP> | + | |
=====10.3 The Cascode===== | =====10.3 The Cascode===== | ||