Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
university:courses:electronics:m2k-spi-debug [02 Apr 2019 16:33] Antoniu Miclausuniversity:courses:electronics:m2k-spi-debug [31 Dec 2020 07:31] (current) – fix links Robin Getz
Line 5: Line 5:
 The objective of this tutorial is to use the Logic Analyzer instrument provided by the [[adi>ADALM2000]] (M2K) board and the [[university:tools:m2k:scopy|Scopy]] software toolset to visualize SPI (Serial Peripheral Interface) transactions between two devices. The objective of this tutorial is to use the Logic Analyzer instrument provided by the [[adi>ADALM2000]] (M2K) board and the [[university:tools:m2k:scopy|Scopy]] software toolset to visualize SPI (Serial Peripheral Interface) transactions between two devices.
  
-The [[resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0411|Total Dissolved Solids Measurements Demo (TDS)]] project will be used as an example. The project uses the [[http://www.analog.com/en/design-center/reference-designs/hardware-reference-design/circuits-from-the-lab/cn0411|EVAL-CN0411-ARDZ shield]] mounted to the [[adi>EVAL-ADICUP360]] microcontroller board. The shield includes two SPI devices: an [[ADI>AD5683R]], 16-bit, voltage-output DAC, and an [[ADI>AD7124-8]], low noise, low power, 24-bit Sigma-Delta ADC.+The [[resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0411|Total Dissolved Solids Measurements Demo (TDS)]] project will be used as an example. The project uses the [[adi>cn0411|EVAL-CN0411-ARDZ shield]] mounted to the [[adi>EVAL-ADICUP360]] microcontroller board. The shield includes two SPI devices: an [[ADI>AD5683R]], 16-bit, voltage-output DAC, and an [[ADI>AD7124-8]], low noise, low power, 24-bit Sigma-Delta ADC.
  
 The TDS project includes a function to set the DAC voltage and read it back via the ADC, providing a complete example of a SPI transaction for analysis. (for more details on how setup and use the software, please refer to the TDS Demo link above). The TDS project includes a function to set the DAC voltage and read it back via the ADC, providing a complete example of a SPI transaction for analysis. (for more details on how setup and use the software, please refer to the TDS Demo link above).
Line 165: Line 165:
 ====Further Reading:==== ====Further Reading:====
  
-  * [[https://www.analog.com/en/analog-dialogue/articles/introduction-to-spi-interface.html|Analog Dialogue - Introduction to SPI interface]]+  * [[adi>en/analog-dialogue/articles/introduction-to-spi-interface.html|Analog Dialogue - Introduction to SPI interface]]
   * [[resources:eval:sdp:sdp-b:peripherals:spi|SPI: Serial Port Interface]]   * [[resources:eval:sdp:sdp-b:peripherals:spi|SPI: Serial Port Interface]]
   * [[university:tools:m2k|ADALM2000 Overview]]   * [[university:tools:m2k|ADALM2000 Overview]]
university/courses/electronics/m2k-spi-debug.txt · Last modified: 31 Dec 2020 07:31 by Robin Getz