This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:lp_hp_filters [13 Aug 2019 09:24] – LPF and HPF hardware setup and procedure Pop Andreea | university:courses:electronics:lp_hp_filters [20 Aug 2019 11:42] – [Questions:] add Resource files Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
======Activity: | ======Activity: | ||
+ | |||
Line 5: | Line 6: | ||
The objective of this Lab activity is to study the characteristics of passive filters by obtaining the frequency response of low pass RC filter and high pass RL filter. | The objective of this Lab activity is to study the characteristics of passive filters by obtaining the frequency response of low pass RC filter and high pass RL filter. | ||
+ | |||
Line 41: | Line 43: | ||
ADALM2000 Active Learning Module\\ | ADALM2000 Active Learning Module\\ | ||
Solder-less breadboard, and jumper wire kit\\ | Solder-less breadboard, and jumper wire kit\\ | ||
- | ADALM1000 hardware module\\ | ||
1 1 KΩ resistor\\ | 1 1 KΩ resistor\\ | ||
1 1 µF capacitor\\ | 1 1 µF capacitor\\ | ||
Line 48: | Line 49: | ||
====Hardware setup:==== | ====Hardware setup:==== | ||
On the solderless breadboard build the circuit presented in Figure 4. | On the solderless breadboard build the circuit presented in Figure 4. | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | |||
====Procedure: | ====Procedure: | ||
To analyze the filter transfer function you must use the Network Analyzer tool. Compute the cutoff frequency of the filter using equation (1). According to this you will set the start and stop frequencies of the logarithmic sweep. In this case the cutoff frequency is 160 Hz. In the network analyzer set the start frequency at 1 Hz and the stop frequency at 10 KHz. Set the minimum phase at -90 the maximum phase at 90. Magnitude axis can be set from -50 dB to 10dB. In Figure 6 is presented the transfer function of the filter obtained by running the network analyzer. | To analyze the filter transfer function you must use the Network Analyzer tool. Compute the cutoff frequency of the filter using equation (1). According to this you will set the start and stop frequencies of the logarithmic sweep. In this case the cutoff frequency is 160 Hz. In the network analyzer set the start frequency at 1 Hz and the stop frequency at 10 KHz. Set the minimum phase at -90 the maximum phase at 90. Magnitude axis can be set from -50 dB to 10dB. In Figure 6 is presented the transfer function of the filter obtained by running the network analyzer. | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
Further you can use the signal generator and the oscilloscope to observe how the filter affects the input signal. On the channel 1 of the signal generator generate a sine waveform with a frequency lower than the cutoff frequency, for example 50 Hz. | Further you can use the signal generator and the oscilloscope to observe how the filter affects the input signal. On the channel 1 of the signal generator generate a sine waveform with a frequency lower than the cutoff frequency, for example 50 Hz. | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
If the frequency of the input signal increases to a value greater than the cutoff frequency, for example 500Hz in this case, you will see an attenuation and a phase difference on the output signal according to the filter transfer function. | If the frequency of the input signal increases to a value greater than the cutoff frequency, for example 500Hz in this case, you will see an attenuation and a phase difference on the output signal according to the filter transfer function. | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
=====B. RL High-pass filter===== | =====B. RL High-pass filter===== | ||
+ | |||
====Hardware setup:==== | ====Hardware setup:==== | ||
On the solderless breadboard build the circuit presented in Figure 9. | On the solderless breadboard build the circuit presented in Figure 9. | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | |||
====Procedure: | ====Procedure: | ||
The procedure is similar to the LPF case. After computing the cutoff frequency using equation (2) set the sweep parameters accordingly. The logarithmic sweep can start in this case at 1 KHz and stop at 100kHz. Phase and magnitude axes can be kept as the same values as in the LPF case. Run the network analyzer to obtain the transfer function as presented in Figure 11. | The procedure is similar to the LPF case. After computing the cutoff frequency using equation (2) set the sweep parameters accordingly. The logarithmic sweep can start in this case at 1 KHz and stop at 100kHz. Phase and magnitude axes can be kept as the same values as in the LPF case. Run the network analyzer to obtain the transfer function as presented in Figure 11. | ||
+ | |||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
- | As in the previous case, generate a sinusoidal waveform on the channel 1 of the signal generator. Observe how at a frequency values lower than the cutoff frequency the output signal is attenuated. | + | |
+ | As in the previous case, generate a sinusoidal waveform on the channel 1 of the signal generator. Observe how at frequency values lower than the cutoff frequency the output signal is attenuated. | ||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
- | If the frequency is higher than the cutoff frequency, the signal is in the pass-band of the filter and the attenuation tends to 0dB. | + | |
+ | If the frequency is higher than the cutoff frequency, the signal is in the pass-band of the filter and the attenuation tends to be 0dB. | ||
{{ : | {{ : | ||
+ | |||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
=====Questions: | =====Questions: | ||
Line 87: | Line 118: | ||
<WRAP round download> | <WRAP round download> | ||
**Lab Resources: | **Lab Resources: | ||
- | * Fritzing files: | + | * Fritzing files: |
- | * LTSpice files: | + | * LTSpice files: |
</ | </ | ||