This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:labs [19 Jul 2017 15:21] – add PV lab Doug Mercer | university:courses:electronics:labs [09 Oct 2017 17:15] – [ADALM2000 Based Lab Activity Material, Electronics I and II] Doug Mercer | ||
---|---|---|---|
Line 5: | Line 5: | ||
The laboratory activities provided on this wiki are considered open source and available for free use in non-commercial educational and academic settings. **The only requirement is that they continue to retain the attribution to Analog Devices Inc.** Supplying them on the ADI wiki allows registered users to contribute to the materials posted here improving the content and keeping them up to date. | The laboratory activities provided on this wiki are considered open source and available for free use in non-commercial educational and academic settings. **The only requirement is that they continue to retain the attribution to Analog Devices Inc.** Supplying them on the ADI wiki allows registered users to contribute to the materials posted here improving the content and keeping them up to date. | ||
- | In general these labs can be performed using the [[university: | + | In general these labs can be performed using the [[university: |
+ | |||
+ | They are generally written to be performed | ||
===Pre-Lab Circuit Simulation=== | ===Pre-Lab Circuit Simulation=== |