This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:labs [28 Jun 2018 16:32] – [Power Management Circuits] add Buck Converter Basics Antoniu Miclaus | university:courses:electronics:labs [04 Oct 2018 16:25] – add wiki Parts Kit link Antoniu Miclaus | ||
---|---|---|---|
Line 7: | Line 7: | ||
In general these labs can be performed using the [[university: | In general these labs can be performed using the [[university: | ||
- | They are generally written to be performed with just the components provided in the [[adi>ADALP2000]] Analog Parts Kit, however additional devices are sometimes needed. Other sources of components can of course be used and there is additional information on that further down on this page. If you are looking for Lab Activity material written specifically for use with the [[university: | + | They are generally written to be performed with just the components provided in the [[university: |
====Pre-Lab Circuit Simulation==== | ====Pre-Lab Circuit Simulation==== |