This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:labs [16 Oct 2015 21:22] – [Analog Discovery Based Lab Activity Material, Electronics I and II] Doug Mercer | university:courses:electronics:labs [23 Mar 2017 15:25] – [Analog Discovery Based Lab Activity Material, Electronics I and II] Doug Mercer | ||
---|---|---|---|
Line 5: | Line 5: | ||
The laboratory activities provided on this wiki are considered open source and available for free use in non-commercial educational and academic settings. **The only requirement is that they continue to retain the attribution to Analog Devices Inc.** Supplying them on the ADI wiki allows registered users to contribute to the materials posted here improving the content and keeping them up to date. | The laboratory activities provided on this wiki are considered open source and available for free use in non-commercial educational and academic settings. **The only requirement is that they continue to retain the attribution to Analog Devices Inc.** Supplying them on the ADI wiki allows registered users to contribute to the materials posted here improving the content and keeping them up to date. | ||
- | In general these labs can be performed using the Analog Discovery module with just the components provided in the Analog Parts Kits supplied by [[http:// | + | In general these labs can be performed using the Analog Discovery module with just the components provided in the ADALP2000 |
===Pre-Lab Circuit Simulation=== | ===Pre-Lab Circuit Simulation=== |