Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revisionBoth sides next revision
university:courses:electronics:labs [31 May 2015 19:56] – [Lab Activity Material Outline, Electronics I and II] Doug Merceruniversity:courses:electronics:labs [16 Oct 2015 21:22] – [Analog Discovery Based Lab Activity Material, Electronics I and II] Doug Mercer
Line 5: Line 5:
 The laboratory activities provided on this wiki are considered open source and available for free use in non-commercial educational and academic settings. **The only requirement is that they continue to retain the attribution to Analog Devices Inc.** Supplying them on the ADI wiki allows registered users to contribute to the materials posted here improving the content and keeping them up to date.  The laboratory activities provided on this wiki are considered open source and available for free use in non-commercial educational and academic settings. **The only requirement is that they continue to retain the attribution to Analog Devices Inc.** Supplying them on the ADI wiki allows registered users to contribute to the materials posted here improving the content and keeping them up to date. 
  
-In general these labs can be performed using the Analog Discovery module with just the components provided in the Analog Parts Kits supplied by [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,842,845&Prod=APK|Digilent]] however additional devices are sometimes needed. Other sources of components can of course be used and there is additional information on that further down on this page.+In general these labs can be performed using the Analog Discovery module with just the components provided in the Analog Parts Kits supplied by [[http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,842,845&Prod=APK|Digilent]] however additional devices are sometimes needed. Other sources of components can of course be used and there is additional information on that further down on this page. If you are looking for Lab Activity material written for use with the [[university:courses:alm1k:alm-labs-list|ADALM1000 look here]].
  
 ===Pre-Lab Circuit Simulation=== ===Pre-Lab Circuit Simulation===
university/courses/electronics/labs.txt · Last modified: 01 Nov 2021 18:20 by Mark Thoren