This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-window-comp-tmp01 [07 Mar 2018 12:20] – add hardware setup and procedure Antoniu Miclaus | university:courses:electronics:electronics-lab-window-comp-tmp01 [07 Mar 2018 13:14] – Antoniu Miclaus | ||
---|---|---|---|
Line 20: | Line 20: | ||
===== Window Comparator ===== | ===== Window Comparator ===== | ||
+ | |||
==== Background ==== | ==== Background ==== | ||
Line 61: | Line 62: | ||
On the plot the " | On the plot the " | ||
+ | |||
+ | ===== Temperature Control ===== | ||
+ | |||
+ | ==== Background ==== | ||
+ | |||
+ | An example of a window comparator application is a simple temperature controller circuit (Figure 2). The temperature sensor, TMP01, has the dual comparator configuration of figure 1 built in. By choosing the proper values for R< | ||
+ | |||
+ | The TMP01 is a linear voltage-output temperature sensor, with a window comparator that can be programmed by the user to activate one of two open-collector outputs when a predetermined temperature set point voltage has been exceeded. A low drift voltage reference is available for set point programming. By connecting the two open collector outputs together as a single wire OR output we can obtain a signal which is at a logic high when the ambient temperature is within the target window. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Programming TMP01 ==== | ||
+ | |||
+ | In the basic fixed set point application utilizing a simple resistor ladder voltage divider, the desired temperature set points are programmed in the following sequence: | ||
+ | |||
+ | 1. Select the desired hysteresis temperature. | ||
+ | |||
+ | 2. Calculate the hysteresis current I< | ||
+ | |||
+ | 3. Select the desired set point temperatures. | ||
+ | |||
+ | 4. Calculate the individual resistor divider ladder values needed to develop the desired comparator set point voltages at SET HIGH and SET LOW. | ||
+ | |||
+ | The hysteresis current is readily calculated. For example, for 2 degrees of hysteresis, I< | ||
+ | |||
+ | V< | ||
+ | |||
+ | V< | ||
+ | |||
+ | R< | ||
+ | |||
+ | R< | ||
+ | |||
+ | R< | ||
+ | |||
+ | The total R< | ||
+ | |||
+ | I< | ||