Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:courses:electronics:electronics-lab-variable-gain-amplifier [26 Mar 2018 13:48] – add Questions and Further Reading Antoniu Miclausuniversity:courses:electronics:electronics-lab-variable-gain-amplifier [03 Jan 2021 22:21] (current) – fix links Robin Getz
Line 26: Line 26:
 Consider the circuit schematic presented in Figure 1. Consider the circuit schematic presented in Figure 1.
  
-<WRAP centeralign> {{:university:courses:electronics:var_gain_amp_crl-sch.png|}} </WRAP>+<WRAP centeralign> {{ :university:courses:electronics:vctrl_amp_transistor.png|}} </WRAP>
  
 <WRAP centeralign> Figure 1. Voltage control using transistor </WRAP> <WRAP centeralign> Figure 1. Voltage control using transistor </WRAP>
Line 42: Line 42:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude peak-to-peak, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 An animated plot is presented in Figure 3. An animated plot is presented in Figure 3.
Line 58: Line 58:
 Consider the circuit schematic presented in Figure 4. Consider the circuit schematic presented in Figure 4.
  
-<WRAP centeralign> {{:university:courses:electronics:var_gain_amp_pot2-sch.png?500|}} </WRAP>+<WRAP centeralign> {{ :university:courses:electronics:var_g_invert_amp_pot.png|}} </WRAP>
  
 <WRAP centeralign> Figure 4. Variable Gain Inverting Amplifier using potetiometer </WRAP> <WRAP centeralign> Figure 4. Variable Gain Inverting Amplifier using potetiometer </WRAP>
Line 74: Line 74:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit.  Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude peak-to-peak, 1 kHz sine wave excitation to the circuit.  Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 By varying the value of the potentiometer, an animated plot is presented in Figure 6. By varying the value of the potentiometer, an animated plot is presented in Figure 6.
Line 90: Line 90:
 Consider the circuit schematic presented in Figure 7. Consider the circuit schematic presented in Figure 7.
  
-<WRAP centeralign> {{:university:courses:electronics:var_gain_amp_pot-sch.png?500|}} </WRAP>+<WRAP centeralign> {{ :university:courses:electronics:var_gain_inv_noninv.png|}} </WRAP>
  
 <WRAP centeralign> Figure 7. Variable Gain Inverting/Non-Inverting Amplifier using potetiometer </WRAP> <WRAP centeralign> Figure 7. Variable Gain Inverting/Non-Inverting Amplifier using potetiometer </WRAP>
Line 106: Line 106:
 ==== Procedure ==== ==== Procedure ====
  
-Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit.  Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.+Use the first waveform generator as source Vin to provide a 2V amplitude peak-to-peak, 1 kHz sine wave excitation to the circuit.  Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2.
  
 By varying the value of the potentiometer, an animated plot is presented in Figure 9. By varying the value of the potentiometer, an animated plot is presented in Figure 9.
Line 125: Line 125:
  
 ===== Further Reading ===== ===== Further Reading =====
 +
 +<WRAP round download>
 +**Lab Resources:**
 +  * Fritzing files: [[downgit>education_tools/tree/master/m2k/fritzing/var_gain_amp_bb | var_gain_amp_bb]]
 +  * LTspice files: [[downgit>education_tools/tree/master/m2k/ltspice/var_gain_amp_ltspice | var_gain_amp_ltspice]]
 +</WRAP>
  
 Some additional resources: Some additional resources:
-  * [[http://www.analog.com/en/analog-dialogue/articles/x-amp-45-db-500-mhz-variable-gain-amplifier.html|X-Amp™, A New 45-dB, 500-MHz Variable-Gain Amplifier (VGA) Simplifies Adaptive Receiver Designs]] +  * [[adi>en/analog-dialogue/articles/x-amp-45-db-500-mhz-variable-gain-amplifier.html|X-Amp™, A New 45-dB, 500-MHz Variable-Gain Amplifier (VGA) Simplifies Adaptive Receiver Designs]] 
-  * [[http://www.analog.com/en/analog-dialogue/articles/reinvent-the-signal-generator.html|Two New Devices Help Reinvent the Signal Generator]]+  * [[adi>en/analog-dialogue/articles/reinvent-the-signal-generator.html|Two New Devices Help Reinvent the Signal Generator]]
  
 **Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]** **Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]**
university/courses/electronics/electronics-lab-variable-gain-amplifier.1522064912.txt.gz · Last modified: 26 Mar 2018 13:48 by Antoniu Miclaus