This shows you the differences between two versions of the page.
Next revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-variable-gain-amplifier [26 Mar 2018 10:39] – created Antoniu Miclaus | university:courses:electronics:electronics-lab-variable-gain-amplifier [15 Jul 2019 17:03] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Activity: Variable Gain Amplifiers ====== | ====== Activity: Variable Gain Amplifiers ====== | ||
- | ===== Objective: ===== | + | ===== Objective ===== |
In this laboratory we continue our discussion on operational amplifiers (see the previous lab here: [[university: | In this laboratory we continue our discussion on operational amplifiers (see the previous lab here: [[university: | ||
Line 8: | Line 8: | ||
A variable-gain or voltage-controlled amplifier is an electronic amplifier that varies its gain depending on a control voltage. This type of circuit has many applications, | A variable-gain or voltage-controlled amplifier is an electronic amplifier that varies its gain depending on a control voltage. This type of circuit has many applications, | ||
+ | |||
+ | ===== Materials ===== | ||
+ | |||
+ | ADALM2000 Active Learning Module\\ | ||
+ | Solder-less breadboard, and jumper wire kit\\ | ||
+ | 2 1 kΩ resistor\\ | ||
+ | 1 4.7 kΩ resistors\\ | ||
+ | 3 10 kΩ resistors\\ | ||
+ | 1 10 kΩ potentiometer\\ | ||
+ | 1 OP97 operational amplifier\\ | ||
+ | 1 2N3904 npn transistor\\ | ||
+ | |||
+ | ===== Voltage Controlled Amplifier using transistor ===== | ||
+ | |||
+ | ==== Background ==== | ||
+ | |||
+ | Consider the circuit schematic presented in Figure 1. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The configuration of the circuit is similar to a basic non-inverting amplifier. The only addition consists of a transistor and a resistor in parallel with resistor R2. The transistor works as a switch that allows 2 gain settings, based on its current state (on/off). | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | |||
+ | Build the following breadboard circuit for the voltage-controlled amplifier using transistors. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Procedure ==== | ||
+ | |||
+ | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. Use the second waveform generator for controlling the transistor, providing a 2V amplitude, 1Hz square wave excitation. Supply the op amp to +/- 5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2. | ||
+ | |||
+ | An animated plot is presented in Figure 3. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The output signal varies between two values, determined by the two gain settings, based on the state of the controlled transistor. | ||
+ | |||
+ | ===== Variable Gain Inverting Amplifier using potetiometer ===== | ||
+ | |||
+ | ==== Background ==== | ||
+ | |||
+ | Consider the circuit schematic presented in Figure 4. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | On the inverting amplifier a potentiometer is used to control manually the output voltage, replacing the standard feedback resistor. | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | |||
+ | Build the following breadboard circuit for the voltage-controlled amplifier using transistors. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Procedure ==== | ||
+ | |||
+ | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. | ||
+ | |||
+ | By varying the value of the potentiometer, | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Using this type of configuration, | ||
+ | |||
+ | ===== Variable Gain Inverting/ | ||
+ | |||
+ | ==== Background ==== | ||
+ | |||
+ | Consider the circuit schematic presented in Figure 7. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | In this amplifier configuration a potentiometer is used to control manually the output voltage, being able to invert the input by adjusting properly the potentiometer. | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | |||
+ | Build the following breadboard circuit for the voltage-controlled amplifier using transistors. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Procedure ==== | ||
+ | |||
+ | Use the first waveform generator as source Vin to provide a 2V amplitude, 1 kHz sine wave excitation to the circuit. | ||
+ | |||
+ | By varying the value of the potentiometer, | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | Using this configuration, | ||
+ | |||
+ | ===== Questions ===== | ||
+ | |||
+ | 1. Which are the gain values for each of the circuits used in this lab activity? | ||
+ | |||
+ | 2. Based on the input signals and the computed gains, which are the expected output values? Compute and compare them with the measured values. | ||
+ | |||
+ | 3. Considering the circuit in Figure 7, how can you increase the output range above +-Vin? | ||
+ | |||
+ | ===== Further Reading ===== | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Lab Resources: | ||
+ | * Fritzing files: [[ https:// | ||
+ | * LTspice files: [[ https:// | ||
+ | </ | ||
+ | |||
+ | Some additional resources: | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | **Return to Lab Activity [[university: | ||
+ | |||
+ | |||
+ |