This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-pulse-width-modulation [19 Apr 2018 09:32] – add schematic Antoniu Miclaus | university:courses:electronics:electronics-lab-pulse-width-modulation [03 Jan 2021 22:21] – fix links Robin Getz | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Objective ===== | ===== Objective ===== | ||
- | In this laboratory we examine | + | In this laboratory we examine pulse width modulation and its usage within a variety of applications. |
- | Pulse Width Modulation (PWM) Signal | + | Pulse Width Modulation (PWM) is a method for encoding |
+ | |||
+ | It is used in transmission of information by encoding a message into a pulsing signal, also for power control of electronic devices such as motors and as principal algorithm for photo-voltaic solar battery chargers. | ||
The __duty cycle__ describes the amount of time the signal is in a high (on) state as a percentage of the total time of it takes to complete one cycle. | The __duty cycle__ describes the amount of time the signal is in a high (on) state as a percentage of the total time of it takes to complete one cycle. | ||
Line 17: | Line 19: | ||
The __frequency__ determines how fast the PWM completes a cycle, and therefore how fast it switches between high and low states. | The __frequency__ determines how fast the PWM completes a cycle, and therefore how fast it switches between high and low states. | ||
- | By varying a digital signal off and on at a fast enough rate, and with a certain duty cycle, the output will appear to behave like a constant voltage analog signal when providing power to devices. | + | By varying a digital signal off and on at a fast-enough rate, and with a certain duty cycle, the output will appear to behave like a constant voltage analog signal when providing power to devices |
- | + | ||
- | The PWM is a technique used in transmission of information by encoding a message into a pulsing signal, also for power control of electronic devices | + | |
===== Materials ===== | ===== Materials ===== | ||
- | ADALM2000 Active Learning Module | ||
- | Solder-less breadboard, and jumper wire kit | ||
- | 1 OP97 operational amplifier | ||
- | ===== Pulse Width Control using Reference Voltage===== | + | ADALM2000 Active Learning Module\\ |
+ | Solder-less breadboard, and jumper wire kit\\ | ||
+ | 1 OP97 operational amplifier\\ | ||
+ | 1 1kΩ resistor | ||
+ | 1 10kΩ potentiometer | ||
- | ==== Background | + | ===== Pulse Width Modulator - Principle of operation |
+ | |||
+ | Pulse Width Modulation (PWM) is a technique to generate low frequency output signals from high frequency pulses. Rapidly switching the output voltage of an inverter leg between the upper and lower DC rail voltages, the low frequency output can be thought of as the average of voltage over a switching period. | ||
+ | |||
+ | Besides that, there are also other several ways of generating pulse-width modulated signals, including analog techniques, sigma-delta modulation, and direct digital synthesis. | ||
+ | |||
+ | One of the simplest methods of generating a PWM signal is to compare two control signals, a carrier signal and a modulation signal. This is known as carrier-based PWM. The carrier signal is a high frequency (switching frequency) triangular waveform. The modulation signal can be any shape. | ||
- | For this particular application we will use a simple operational amplifier in a switching mode configuration (see [[university: | + | Using this approach, the output waveform can be a PWM representation |
Consider the circuit in Figure 1. | Consider the circuit in Figure 1. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | Following the description of the PWM principle, we use the negative input of the operational amplifier for carrier, while the positive input for the modulation signal. Thus, a higher modulation signal will result in an output that is at a high level for a greater fraction of the PWM period. | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | |||
+ | Build the following breadboard circuit for Pulse Width Modulation. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Procedure ==== | ||
+ | |||
+ | Use the first waveform generator as the carrier signal providing a 4V amplitude peak-to-peak, | ||
+ | |||
+ | Supply the op amp with +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2 . | ||
+ | |||
+ | In the figure there are presented the two signal generator channels containing the two input signals (orange - carrier signal, purple - modulation signal). | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | A plot of the output signal on channel 2 of the scope is presented in Figure 4. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | If the instantaneous magnitude of the modulation signal is greater than the carrier signal at a point in time, the output will be high. If the modulation signal is lower than the carrier signal, the output will be low. | ||
+ | |||
+ | If the peak of the modulation is less than the peak of the carrier signal, the output will be a faithful PWM representation of the modulation signal. Edit | ||
+ | |||
+ | ===== Pulse Width Control using a DC modulation Voltage===== | ||
+ | |||
+ | ==== Background ==== | ||
+ | |||
+ | For this particular application we will use a simple operational amplifier in a switching mode configuration (see [[university: | ||
+ | |||
+ | Consider the circuit in Figure 5. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
The circuit works as a simple comparator where the negative input of the operational amplifier is connected to the | The circuit works as a simple comparator where the negative input of the operational amplifier is connected to the | ||
- | input waveform, while the positive input acts as a threshold voltage which establishes when the transitions between high voltage output and low voltage output occur. The potentiometer acts as a voltage divider for the input reference voltage, adjusting the threshold voltage, and implicitly the duty cycle of the output signal. | + | carrier |
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | Build the following breadboard circuit for Pulse Width Control using Reference | + | Build the following breadboard circuit for Pulse Width Control using a DC modulation |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as source Vin to provide a 5V amplitude, 1 kHz triangle wave excitation to the circuit. Use the second waveform generator as constant voltage source with 5V amplitude. | + | Use the first waveform generator as source Vin to provide a 5V amplitude |
Supply the op amp to +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2. | Supply the op amp to +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal is displayed on channel 2. | ||
- | An animated plot is presented in Figure | + | An animated plot is presented in Figure |
- | The output signal is a squared shaped determined by the two possible output values. We can notice that, by varying the potentiometer value, the duty cycle of the signal changes, while the frequency remains constant. | + | <WRAP centeralign> |
- | ===== Pulse Width Modulation Principle ===== | + | <WRAP centeralign> |
- | Pulse Width Modulation (PWM) is a technique to generate low frequency output signals from high frequency pulses. Rapidly switching | + | The output signal |
- | In its simplest form PWM output signals are constructed by comparing two control signals, a carrier signal and a modulation signal. This is known as carrier-based PWM. The carrier signal is a high frequency (switching frequency) triangular waveform. The modulation signal can be any shape. | + | ===== Fixed 50% PWM with Astable Multivibrator===== |
- | Using this approach, the output waveform can be made to follow any desired waveform shape. With machines, sinusoidal and trapezoidal waveform shapes are among the most common. | + | ==== Background ==== |
- | Consider the circuit in Figure | + | Consider the circuit in Figure |
- | Following | + | <WRAP centeralign> |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The circuit shows an astable multivibrator using a single operational amplifier. The functionality is easy to understand while considering | ||
+ | The input of the Schmitt trigger, which is identical to the inverting | ||
+ | |||
+ | The advantage of this circuit is that it does not require an M2K to generate a carrier (but the duty cycle is fixed at 50%.) | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
- | Build the following breadboard circuit for Pulse Width Modulation. | + | Build the following breadboard circuit for PWM with Astable Multivibrator. |
+ | |||
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
==== Procedure ==== | ==== Procedure ==== | ||
- | Use the first waveform generator as carrier signal providing a 4V amplitude, 2.5V offset, 1 kHz triangle wave excitation to the circuit. Use the second waveform generator as modulation | + | Supply |
- | In the figure there are presented the two signal | + | A plot with the output |
+ | <WRAP centeralign> | ||
+ | <WRAP centeralign> | ||
- | Supply the op amp to +5V from the power supply. Configure the scope so that the input signal is displayed on channel 1 and the output signal | + | Note that the duty cycle of the output signal is approximately around 50% while the low/high voltage values tend to reach the positive/ |
+ | |||
+ | ===== Extra Activity ===== | ||
+ | |||
+ | In the previous example we generated a 50% fixed duty cycle PWM using astable multivibrators. But how can we adjust the duty cycle? For this we will need to alter the circuit slightly. | ||
+ | |||
+ | Consider the circuit presented in Figure 11. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The resistor R< | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | |||
+ | Build the following breadboard circuit for adjusting the duty cycle for PWM with Multivibrators. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | ==== Procedure ==== | ||
+ | |||
+ | Supply the circuit | ||
+ | |||
+ | Vary the potentiometer value and notice the duty cycle change. A plot example is presented in Figure 13. | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | In this example the duty cycle was set to around 25%. Whenever the duty cycle is altered, there is inevitably a slight variation in the switching frequency, because the two coupling networks at the inverting and non-inverting input are both connected to the output of the operational amplifier. | ||
+ | |||
+ | ===== Going Further with the Lab ===== | ||
+ | |||
+ | All the activities in this laboratory are based on a simple op-amp (OP97) configured as comparator. The ADALP2000 Parts Kit contains also the comparator AD8561, designed for this single purpose. Therefore, the performance of the PWM circuits might be increased by using this part. | ||
+ | |||
+ | Build the above discussed circuits using AD8561 from the Parts Kit and discuss any noticeable changes of the circuit behavior and the input/ | ||
- | A plot with the output signal on channel 2 of the scope is presented in Figure 6. | + | <WRAP round download> |
+ | **Lab Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
+ | ===== Further Reading ===== | ||
- | If the peak of the modulation is less than the peak of the carrier signal, the output will follow the shape of the modulation signal. | + | Some additional resources: |
- | If instantaneous magnitude of the modulation signal is greater than the carried signal at a point in time, the output voltage should be connected to positive side of the supply (high state). If the carrier signal is greater than the modulation | + | * [[https:// |
+ | * [[university: | ||
+ | * [[adi> | ||
+ | **Return to Lab Activity [[university: | ||