This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-opamp-comparator [25 Jun 2020 22:07] – external edit | university:courses:electronics:electronics-lab-opamp-comparator [16 May 2022 15:22] (current) – [The op-amp as a "comparator":] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity: Op Amp as Comparator ====== | + | ======Activity: |
===== Objective: ===== | ===== Objective: ===== | ||
Line 15: | Line 15: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Op Amps and comparators may seem interchangeable at first glance based on their symbols and pinouts. The Analog Parts Kits is supplied with a variety of op-amps and the AD8561 high speed voltage comparator that was used in other activities. Some designers might be tempted to use or substitute readily available op amps as voltage comparators in their projects. There are very important differences however. Comparators are designed to work without negative feedback or open-loop, they are generally designed to drive digital logic circuits from their outputs, and they are designed to work at high speed with minimal instability. Op amps are not generally designed for use as comparators, | + | Op Amps and comparators may seem interchangeable at first glance based on their symbols and pinouts. The Analog Parts Kits is supplied with a variety of op-amps and the AD8561 high speed voltage comparator that was used in other activities. Some designers might be tempted to use or substitute readily available op amps as voltage comparators in their projects. There are very important differences however. Comparators are designed to work without negative feedback or open-loop, they are generally designed to drive digital logic circuits from their outputs, and they are designed to work at high speed with minimal instability. Op amps are not generally designed for use as comparators, |
<note important> | <note important> | ||
Line 281: | Line 281: | ||
Some additional resources on Op Amps as Comparators: | Some additional resources on Op Amps as Comparators: | ||
- | * [[http:// | + | * [[adi>media/ |
- | * [[http:// | + | * [[adi>en/ |
- | * [[http:// | + | * [[adi>en/ |
- | * [[http:// | + | * [[adi>en/ |
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||