Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
university:courses:electronics:electronics-lab-opamp-comparator [16 Feb 2020 21:14] – [The op-amp as a "comparator":] Doug Mercer | university:courses:electronics:electronics-lab-opamp-comparator [03 Nov 2021 20:27] – [Activity: Op Amp as Comparator] Doug Mercer |
---|
====== Activity: Op Amp as Comparator ====== | ======Activity: Op Amp as Comparator, For ADALM2000====== |
| |
===== Objective: ===== | ===== Objective: ===== |
<WRAP centeralign>Figure 1a, An op-amp used as a comparator</WRAP> | <WRAP centeralign>Figure 1a, An op-amp used as a comparator</WRAP> |
| |
Op Amps and comparators may seem interchangeable at first glance based on their symbols and pinouts. The Analog Parts Kits is supplied with a variety of op-amps and the AD8561 high speed voltage comparator that was used in the earlier activities. Some designers might be tempted to use or substitute readily available op amps as voltage comparators in their projects. There are very important differences however. Comparators are designed to work without negative feedback or open-loop, they are generally designed to drive digital logic circuits from their outputs, and they are designed to work at high speed with minimal instability. Op amps are not generally designed for use as comparators, their input structures may saturate if over-driven which may cause it to respond comparatively slowly. Many have input stages which behave in unexpected ways when driven with large differential voltages or beyond the specified common mode range. In fact, in many cases, the differential input voltage range of an op amp is limited or clamped to prevent damage to the input stage devices. | Op Amps and comparators may seem interchangeable at first glance based on their symbols and pinouts. The Analog Parts Kits is supplied with a variety of op-amps and the AD8561 high speed voltage comparator that was used in other activities. Some designers might be tempted to use or substitute readily available op amps as voltage comparators in their projects. There are very important differences however. Comparators are designed to work without negative feedback or open-loop, they are generally designed to drive digital logic circuits from their outputs, and they are designed to work at high speed with minimal instability. Op amps are not generally designed for use as comparators, their input structures may saturate if over-driven which may cause it to respond comparatively slowly. Many have input stages which behave in unexpected ways when driven with large differential voltages or beyond the specified common mode range. In fact, in many cases, the differential input voltage range of an op amp is limited or clamped to prevent damage to the input stage devices. |
| |
<note important>Warning: Using op-amps with built-in input clamps as a voltage comparator may damage the IC!</note> | <note important>Warning: Using op-amps with built-in input clamps as a voltage comparator may damage the IC!</note> |
| |
Yet many designers still try to use op amps as comparators. While this may work at low speeds and low resolutions, many times the results are not satisfactory. Not all of the issues involved with using an op amp as a comparator can be resolved by reference to the op amp datasheet, since op amps are not intended for use as comparators. | Yet many designers still try to use op amps as comparators. While this may work in some cases at low speeds and low resolutions, many times the results are not satisfactory. Not all of the issues involved with using an op amp as a comparator can be resolved by reference to the op amp datasheet, since op amps are not intended for use as comparators. |
| |
The most common issues are speed (as we have already mentioned), the effects of input structures (protection diodes, phase inversion in FET amplifiers such as the ADTL082, and many others), output structures which are not intended to drive logic, hysteresis and stability, and common-mode effects. | The most common issues are speed (as we have already mentioned), the effects of input structures (protection diodes, phase inversion in FET amplifiers such as the ADTL082, and many others), output structures which are not intended to drive logic, hysteresis and stability, and common-mode effects. |
<WRAP round download> | <WRAP round download> |
** Lab Resources:** | ** Lab Resources:** |
* LTSpice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/opamp_comp_ltspice | opamp_comp_ltspice]] | * LTSpice files: [[downgit>education_tools/tree/master/m2k/ltspice/opamp_comp_ltspice | opamp_comp_ltspice]] |
* Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/opamp_comp_bb | opamp_comp_bb]] | * Fritzing files: [[downgit>education_tools/tree/master/m2k/fritzing/opamp_comp_bb | opamp_comp_bb]] |
</WRAP> | </WRAP> |
| |
| |
Some additional resources on Op Amps as Comparators: | Some additional resources on Op Amps as Comparators: |
* [[http://www.analog.com/media/en/technical-documentation/application-notes/AN-849.pdf|AN-849 - Using Op Amps as Comparators]] | * [[adi>media/en/technical-documentation/application-notes/AN-849.pdf|AN-849 - Using Op Amps as Comparators]] |
* [[http://www.analog.com/en/analog-dialogue/articles/amplifiers-as-comparators.html|Ask The Applications Engineer—31: Amplifiers as Comparators?]] | * [[adi>en/analog-dialogue/articles/amplifiers-as-comparators.html|Ask The Applications Engineer—31: Amplifiers as Comparators?]] |
* [[http://www.analog.com/en/analog-dialogue/articles/curing-comparator-instability-with-hysteresis.html|Curing Comparator Instability with Hysteresis]] | * [[adi>en/analog-dialogue/articles/curing-comparator-instability-with-hysteresis.html|Curing Comparator Instability with Hysteresis]] |
* [[http://www.analog.com/en/analog-dialogue/raqs/raq-issue-11.html|Comparators & Op Amps—May They Never Meet]] | * [[adi>en/analog-dialogue/raqs/raq-issue-11.html|Comparators & Op Amps—May They Never Meet]] |
| |
| |
**Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]** | **Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]** |
| |