Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:courses:electronics:electronics-lab-opamp-comparator [26 Oct 2018 12:40] – [Further Reading] add Fritzing files Antoniu Miclaus | university:courses:electronics:electronics-lab-opamp-comparator [05 Mar 2019 10:52] – [Further Reading] Antoniu Miclaus |
---|
===== Hysteresis Comparator ===== | ===== Hysteresis Comparator ===== |
| |
Hysteresis is considered to be a phenomenon according to which the actual value of a quantity (material) depends on a previous values of quantities determining it. It is aproperty of a system such that an output value is not a strict function of the corresponding input, but also incorporates some lag, delay, or history dependence, and in particular the response for a decrease in the input variable is different from the response for an increase in the input variable. | Hysteresis is the dependence of a system's current state on previous values of quantities determining it. The output value is not a strict function of the corresponding input, but also incorporates some lag, delay, or history dependence. In particular, the response for a decrease in the input variable is different from the response for an increase in the input variable. |
| |
In this configuration, there are two threshold values V<sub>ThH</sub> and V<sub>ThL</sub> with two output values V<sub>OH</sub> and V<sub>OL</sub>. The threshold values should depend on the output value which is fed back to the input and contributes to the threshold values (positive feedback). Via a resistive divider, a fraction of the output voltage is fed back to the non-inverting input. | In this configuration, there are two threshold values V<sub>ThH</sub> and V<sub>ThL</sub> with two output values V<sub>OH</sub> and V<sub>OL</sub>. The threshold values should depend on the output value which is fed back to the input and contributes to the threshold values (positive feedback). Via a resistive divider, a fraction of the output voltage is fed back to the non-inverting input. |
This type of circuit is also known as Window Comparator. An an application on this subject can be found in the activity: [[university:courses:electronics:electronics-lab-window-comp-tmp01|Temperature Control using Window Comparator]] | This type of circuit is also known as Window Comparator. An an application on this subject can be found in the activity: [[university:courses:electronics:electronics-lab-window-comp-tmp01|Temperature Control using Window Comparator]] |
| |
==== Further Reading ==== | <WRAP round download> |
** Lab Resources:** | ** Lab Resources:** |
* LTSpice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/opamp_comp_ltspice | opamp_comp_ltspice]] | * LTSpice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/opamp_comp_ltspice | opamp_comp_ltspice]] |
* Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/opamp_comp_bb | opamp_comp_bb]] | * Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/opamp_comp_bb | opamp_comp_bb]] |
| </WRAP> |
| |
| ==== Further Reading ==== |
| |
Some additional resources on Op Amps as Comparators: | Some additional resources on Op Amps as Comparators: |