This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-led-sensor [27 Mar 2017 16:46] – [Materials:] Doug Mercer | university:courses:electronics:electronics-lab-led-sensor [27 Mar 2017 16:51] – [Hardware Setup:] Doug Mercer | ||
---|---|---|---|
Line 31: | Line 31: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | Use the fixed +5 V power supply from the Discovery | + | Use the variable positive |
=====Procedure: | =====Procedure: |