This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-lco [23 Mar 2017 16:36] – [Directions:] Doug Mercer | university:courses:electronics:electronics-lab-lco [13 Jun 2022 20:07] (current) – [Background:] Doug Mercer | ||
---|---|---|---|
Line 25: | Line 25: | ||
Below in figure 2 is the schematic and pinout for the CD4007: | Below in figure 2 is the schematic and pinout for the CD4007: | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 47: | Line 47: | ||
==== Hardware Setup: ==== | ==== Hardware Setup: ==== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 2.5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. | + | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude |
==== Procedure: ==== | ==== Procedure: ==== | ||
Line 96: | Line 96: | ||
==== Additional Activity: ==== | ==== Additional Activity: ==== | ||
- | Could you modify this circuit to make the frequency of the oscillator temperature dependent by substituting the photo resistor with the thermistor from the Analog Parts Kit? | + | Could you modify this circuit to make the frequency of the oscillator temperature dependent by substituting the photo resistor with the thermistor from the ADALP2000 |
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: |