This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-lco [23 Mar 2017 16:35] – [Materials:] Doug Mercer | university:courses:electronics:electronics-lab-lco [23 Aug 2019 13:59] – Antoniu Miclaus | ||
---|---|---|---|
Line 39: | Line 39: | ||
==== Directions: ==== | ==== Directions: ==== | ||
- | First build the simple example shown in figure 4 to test the input to output transfer function of the CMOS amplifier. The green boxes indicate connections to the connector on Analog Discovery. Connect V+ (+5V) power to V< | + | First build the simple example shown in figure 4 to test the input to output transfer function of the CMOS amplifier. The green boxes indicate connections to the connector on the ADALM2000. Connect V+ (+5V) power to V< |
{{ : | {{ : | ||
Line 47: | Line 47: | ||
==== Hardware Setup: ==== | ==== Hardware Setup: ==== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 2.5V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. | + | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude |
==== Procedure: ==== | ==== Procedure: ==== | ||
Line 96: | Line 96: | ||
==== Additional Activity: ==== | ==== Additional Activity: ==== | ||
- | Could you modify this circuit to make the frequency of the oscillator temperature dependent by substituting the photo resistor with the thermistor from the Analog Parts Kit? | + | Could you modify this circuit to make the frequency of the oscillator temperature dependent by substituting the photo resistor with the thermistor from the ADALP2000 |
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: |