Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
university:courses:electronics:electronics-lab-heartbeat [25 Jan 2022 08:00] – Remove SIMetrix files Monica Ignatuniversity:courses:electronics:electronics-lab-heartbeat [30 Jan 2023 09:19] (current) – [Preamplifier] Antoniu Miclaus
Line 60: Line 60:
  
 The input signal from the heartbeat measurement setup is fed into a Differentiator Amplifier Circuit(([[http://www.electronics-tutorials.ws/opamp/opamp_7.html|Differentiator Amplifier]])) (C<sub>1</sub>, A<sub>1</sub>, R<sub>3</sub>). The capacitor blocks any DC content, C<sub>1</sub> and R<sub>3</sub> behaving as a high pass filter with the cut-off frequency F<sub>c1</sub> being determined by the following formula: The input signal from the heartbeat measurement setup is fed into a Differentiator Amplifier Circuit(([[http://www.electronics-tutorials.ws/opamp/opamp_7.html|Differentiator Amplifier]])) (C<sub>1</sub>, A<sub>1</sub>, R<sub>3</sub>). The capacitor blocks any DC content, C<sub>1</sub> and R<sub>3</sub> behaving as a high pass filter with the cut-off frequency F<sub>c1</sub> being determined by the following formula:
-<WRAP centeralign><m>F_c1=1/{2 pi R_1C_1}</m></WRAP>+<WRAP centeralign><m>F_c1=1/{2 pi R_3C_1}</m></WRAP>
 Besides filtering, this stage serves also as an amplifier taking as input the current (I<sub>A1</sub>), and generating at the output an inverted voltage (V<sub>A1</sub>) based on the negative feedback resistance (R<sub>3</sub>):  Besides filtering, this stage serves also as an amplifier taking as input the current (I<sub>A1</sub>), and generating at the output an inverted voltage (V<sub>A1</sub>) based on the negative feedback resistance (R<sub>3</sub>): 
-<WRAP centeralign><m>V_A1=-I_A1*R_1</m></WRAP>+<WRAP centeralign><m>V_A1=-I_A1*R_3</m></WRAP>
  
 ====Active Low-Pass Filter=== ====Active Low-Pass Filter===
university/courses/electronics/electronics-lab-heartbeat.txt · Last modified: 30 Jan 2023 09:19 by Antoniu Miclaus