This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-external-trigger [05 Mar 2019 12:45] – [Appendix: Making an inverter with the CD4007 transistor array] Antoniu Miclaus | university:courses:electronics:electronics-lab-external-trigger [23 Aug 2019 14:08] – Antoniu Miclaus | ||
---|---|---|---|
Line 33: | Line 33: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | Waveform generator AWG1 should be set up as a triangle wave with a 8 Volt amplitude and 0 V offset and a frequency of 5 KHz. Set the horizontal and vertical scales of the scope to display at least one complete cycle of the input triangle waveform. Turn on the power supplies only after double checking your circuit connections. | + | Waveform generator AWG1 should be set up as a triangle wave with a 8 Volt amplitude |
{{ : | {{ : |