This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-ce-loop-gain [27 Mar 2019 12:05] – [Questions:] add ltspice files Antoniu Miclaus | university:courses:electronics:electronics-lab-ce-loop-gain [26 Jan 2021 15:58] (current) – [Directions:] Doug Mercer | ||
---|---|---|---|
Line 99: | Line 99: | ||
====Directions: | ====Directions: | ||
- | Build the measurement setup as shown in figure 5 below. If you are using the HPH1-1400L transformer for T< | + | Build the measurement setup as shown in figure 5 below. If you are using the HPH1-1400L transformer for T< |
There are three resistors, R< | There are three resistors, R< | ||
Line 117: | Line 117: | ||
The green squares indicate where to connect the ADALM2000 AWG, scope channels and power supplies. Be sure to turn on the power supplies only after you double check your wiring. | The green squares indicate where to connect the ADALM2000 AWG, scope channels and power supplies. Be sure to turn on the power supplies only after you double check your wiring. | ||
- | Open the voltage supply control window to turn on and off the fixed +5 volt power supply. Open the Network Analyzer Instrument and set the sweep to start at 10 KHz and stop at 5 MHz. The Max gain should be set to 0.1X. Set the Amplitude to 3.5 V and the Offset to zero volts. Under the Bode scale set the magnitude top to 40 dB and range to 80 dB. Set the phase top to 180º and range to 360º. Under scope channels click on use channel 1 as reference. Set the number of steps to 500. | + | Open the voltage supply control window to turn on and off the fixed +5 volt power supply. Open the Network Analyzer Instrument and set the sweep to start at 10 KHz and stop at 5 MHz. The Max gain should be set to 0.1X. Set the Amplitude to 3.5 V peak-to-peak |
====Procedure: | ====Procedure: | ||
Line 139: | Line 139: | ||
<WRAP round download> | <WRAP round download> | ||
**Resources: | **Resources: | ||
- | * LTSpice files: [[ https:// | + | * LTSpice files: [[downgit>education_tools/ |
</ | </ | ||