This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-ce-loop-gain [23 Mar 2017 16:04] – [Hardware Setup:] Doug Mercer | university:courses:electronics:electronics-lab-ce-loop-gain [24 Apr 2017 08:26] – rename Antoniu Miclaus | ||
---|---|---|---|
Line 27: | Line 27: | ||
**To Review:** One method to measure the loop gain in negative feedback systems is the voltage injection method. The following shows how the voltage injection method can be applied in practice and what has to be considered to achieve correct results. | **To Review:** One method to measure the loop gain in negative feedback systems is the voltage injection method. The following shows how the voltage injection method can be applied in practice and what has to be considered to achieve correct results. | ||
- | Using a suitable injection transformer ( the Analog Parts kit contains a HPH1-1400L ) we can inject a test voltage at an appropriate injection-point in the feedback loop of the system. Then the response of the loop can be measured using a network analyzer like the Analog Discovery. | + | Using a suitable injection transformer ( the ADALP2000 |
Figure 2 shows a setup using the voltage injection method to measure the loop gain of a feedback system. A low value resistor is inserted in the feedback loop at the injection-point. The injection transformer secondary winding is connected across the injection resistor to apply the test voltage. This allows the injection of a test voltage without changing the DC-bias operating point of the system. | Figure 2 shows a setup using the voltage injection method to measure the loop gain of a feedback system. A low value resistor is inserted in the feedback loop at the injection-point. The injection transformer secondary winding is connected across the injection resistor to apply the test voltage. This allows the injection of a test voltage without changing the DC-bias operating point of the system. | ||
Line 103: | Line 103: | ||
There are three resistors, R< | There are three resistors, R< | ||
- | Voltage divider R< | + | Voltage divider R< |
{{ : | {{ : |