This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-capacitors [08 Feb 2013 21:05] – [CAPACITOR COMPARISON CHART] Doug Mercer | university:courses:electronics:electronics-lab-capacitors [17 Jun 2013 14:45] – minor edit to remove picture reference Doug Mercer | ||
---|---|---|---|
Line 44: | Line 44: | ||
Electrolytic capacitors are polarized and **they must be connected with the correct orientation**, | Electrolytic capacitors are polarized and **they must be connected with the correct orientation**, | ||
- | There are two designs of electrolytic capacitors; **axial** where the leads are attached to each end (220µF in picture) | + | There are two designs of electrolytic capacitors; **axial** where the leads are attached to each end and **radial** where both leads are at the same end. Radial capacitors tend to be a little smaller and they stand upright on the circuit board while axial capacitors can have a lower profile on a PC board but may take up more space. |
{{ : | {{ : |