This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-breadboards [15 Apr 2013 17:03] – [For more on building advanced breadboards see:] Doug Mercer | university:courses:electronics:electronics-lab-breadboards [12 Apr 2017 12:32] – rename Antoniu Miclaus | ||
---|---|---|---|
Line 40: | Line 40: | ||
5. Trimming the leads of components like resistors, capacitors, transistors and LEDs, so that they fit closely to the board and do not get pulled out by accident is a good practice.\\ | 5. Trimming the leads of components like resistors, capacitors, transistors and LEDs, so that they fit closely to the board and do not get pulled out by accident is a good practice.\\ | ||
- | ===== Using breadboards with the Analog Discovery | + | ===== Using breadboards with the ADALM2000 |
- | All the connections to the Analog Discovery | + | All the connections to the ADALM2000 |
- | Adapters such as those shown below are workable alternatives. They adapt the square male pins of the Discovery | + | Adapters such as those shown below are workable alternatives. They adapt the square male pins of the ADALM2000 |
{{: | {{: | ||
- | These adapters can be easily constructed from dual row female receptacles, | + | These adapters can be easily constructed from dual row female receptacles, |
A 12 pin (dual row of six) version is also available from: | A 12 pin (dual row of six) version is also available from: | ||
- | The smaller adapters can be used individually or combined to fill out the entire 30 pins of the Discovery | + | The smaller adapters can be used individually or combined to fill out the entire 30 pins of the ADALM2000 |
- | Another more convenient arrangement would be an adapter PC board that connects to the 30 pin male header of Discovery | + | Another more convenient arrangement would be an adapter PC board that connects to the 30 pin male header of ADALM2000 |
{{ : | {{ : | ||
Line 60: | Line 60: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The board consists of a grid of 21 by 30 plated through holes on 0.1" centers which can be used to solder test circuits. Three of the columns of holes on the left side of the grid are shorted together and tied to the +5V, -5V and ground connections on the 30 pin right angle female connector that mates with Discovery. Three of the columns of holes on the right side of the grid are shorted together and tied to the +9V, -9V and ground connections for use with external batteries or other sources of power. The 30 Discovery | + | The board consists of a grid of 21 by 30 plated through holes on 0.1" centers which can be used to solder test circuits. Three of the columns of holes on the left side of the grid are shorted together and tied to the +5V, -5V and ground connections on the 30 pin right angle female connector that mates with ADALM2000. Three of the columns of holes on the right side of the grid are shorted together and tied to the +9V, -9V and ground connections for use with external batteries or other sources of power. The 30 ADALM2000 |
The 21 X 30 grid is sized to accommodate the popular 30 position (400 total connection points) solder-less breadboards with power busses along both sides which are 2 1/8" by 3 1/4". These breadboards come with adhesive backs that will stick the breadboard to the adapter PC board. | The 21 X 30 grid is sized to accommodate the popular 30 position (400 total connection points) solder-less breadboards with power busses along both sides which are 2 1/8" by 3 1/4". These breadboards come with adhesive backs that will stick the breadboard to the adapter PC board. | ||
- | The schematic of the adapter board is shown in figure 5. The signals and power supplies that Analog Discovery | + | The schematic of the adapter board is shown in figure 5. The signals and power supplies that ADALM2000 |
{{ : | {{ : | ||
Line 68: | Line 68: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | The layout of the resistors around the dual op-amp are arranged such that rather than two independent amplifiers, a single resistor can be inserted between the two inverting inputs, in place of the two resistors (R1,R4) to ground. Configured this way the two op-amps form the input section of an instrumentation amplifier. The amplified differential signal at the outputs of the two amplifiers can then be connected to the differential scope inputs on Discovery. Another possible use would be to generate complementary or differential signals from one of the AWGs. By connecting one input to ground, with the other input connected to one of the AWG outputs and adjusting the resistor values the first amplifier acts as a non-inverting stage to generate the in phase or true output and the other amplifier acts as an inverting stage to generate the 180º phase or complement output. To make it easy to swap resistor values individual pin sockets could be installed rather than directly soldering the resistors to the board. Likewise using a socket for the op-amp would allow you to interchange different devices optimized for the intended application. | + | The layout of the resistors around the dual op-amp are arranged such that rather than two independent amplifiers, a single resistor can be inserted between the two inverting inputs, in place of the two resistors (R1,R4) to ground. Configured this way the two op-amps form the input section of an instrumentation amplifier. The amplified differential signal at the outputs of the two amplifiers can then be connected to the differential scope inputs on ADALM2000. Another possible use would be to generate complementary or differential signals from one of the AWGs. By connecting one input to ground, with the other input connected to one of the AWG outputs and adjusting the resistor values the first amplifier acts as a non-inverting stage to generate the in phase or true output and the other amplifier acts as an inverting stage to generate the 180º phase or complement output. To make it easy to swap resistor values individual pin sockets could be installed rather than directly soldering the resistors to the board. Likewise using a socket for the op-amp would allow you to interchange different devices optimized for the intended application. |
- | The Discovery | + | The ADALM2000 |
Eagle CAD schematic and PCB layout files can be down loaded here {{: | Eagle CAD schematic and PCB layout files can be down loaded here {{: |