This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-breadboard-coupling [12 Apr 2017 12:40] – rename Antoniu Miclaus | university:courses:electronics:electronics-lab-breadboard-coupling [24 Jul 2017 14:58] – change amplitude value to peak-peak Antoniu Miclaus | ||
---|---|---|---|
Line 48: | Line 48: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Using the Network Analyzer instrument in the Scopy software obtain a gain (attenuation) vs. frequency plot from 10 Hz to 10 MHz. Scope channel 1 is the " | + | Using the Network Analyzer instrument in the Scopy software obtain a gain (attenuation) vs. frequency plot from 10 Hz to 10 MHz. Scope channel 1 is the " |
===== Procedure: ===== | ===== Procedure: ===== |