This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-active-mixer [29 Jul 2019 14:04] – Double balanced mixer with LTC1043 Pop Andreea | university:courses:electronics:electronics-lab-active-mixer [30 Jul 2019 08:21] – edited single bal Trecia Agoylo | ||
---|---|---|---|
Line 29: | Line 29: | ||
===== Materials ===== | ===== Materials ===== | ||
+ | ADALM2000 Active Learning Module\\ | ||
+ | Solder-less breadboard, and jumper wire kit\\ | ||
+ | 2 1 kΩ resistor\\ | ||
+ | 2 6.8k kΩ resistor\\ | ||
+ | 1 OP37 precision op-amp\\ | ||
+ | 1 LTC1043 precision switched-cap block \\ | ||
+ | 3 N-channel MOSFET\\ | ||
=====Single Balanced Active Mixer===== | =====Single Balanced Active Mixer===== | ||
Line 36: | Line 43: | ||
A single-balanced mixer often called a balanced mixer, is a type of mixer which suppresses either the LO or RF signal but not both. This configuration is hardly used because of its susceptibility to noise in the input LO signal. The main drawback is its IF-LO feed-through, | A single-balanced mixer often called a balanced mixer, is a type of mixer which suppresses either the LO or RF signal but not both. This configuration is hardly used because of its susceptibility to noise in the input LO signal. The main drawback is its IF-LO feed-through, | ||
- | {{ : | + | {{ : |
< | < | ||
Line 42: | Line 49: | ||
====Hardware Setup==== | ====Hardware Setup==== | ||
- | Build the following breadboard connection shown in Figure | + | Build the following breadboard connection shown in Figure |
{{ : | {{ : | ||
Line 49: | Line 56: | ||
====Procedure==== | ====Procedure==== | ||
- | Use Signal Generator | + | Use Signal Generator W1 and W2, as the frequency inputs to the mixer. For the LO frequency use W1, set it to 5V 210 kHz sine wave. For the RF input, use W2. |
- | For the Up-conversion mixing, set Signal Generator Ch1 to 5V, 500kHz | + | For the Up-conversion mixing, W2 should be lower than the LO frequency |
- | Probe Analog | + | |
- | {{ : | + | {{ : |
< | < | ||
- | For the Down-conversion mixing, set Signal Generator Ch1 to 5V, 500kHz sine wave, this will serve as the LO frequency for this activity. Then, set Signal Generator Ch2 to 5V, 490kHz | + | For the Down-conversion mixing, set W2 to 5V, 260kHz |
- | {{ : | + | {{ : |
< | < | ||
+ | |||
===== Single balanced active mixer implemented with LTC1043 ===== | ===== Single balanced active mixer implemented with LTC1043 ===== |