This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-8m [23 Mar 2017 16:11] – [Materials:] Doug Mercer | university:courses:electronics:electronics-lab-8m [23 Aug 2019 12:54] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: Stabilized current source (NMOS) ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 24: | Line 24: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 1 KHz triangle wave with 2 volt amplitude and 2V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the drain of M< | + | {{: |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The waveform generator should be configured for a 1 KHz triangle wave with 4 volt amplitude | ||
===== Procedure: | ===== Procedure: | ||
Line 30: | Line 34: | ||
The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the drain of transistor M< | The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the drain of transistor M< | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | <WRAP centeralign> | ||
===== Questions: ===== | ===== Questions: ===== | ||
Line 44: | Line 50: | ||
The output current has a narrow peak. How could multiple copies of the peaking current source be combined to produce a much wider, flatter peak? | The output current has a narrow peak. How could multiple copies of the peaking current source be combined to produce a much wider, flatter peak? | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * LTspice files: [[ https:// | ||
+ | * Fritzing files: [[ https:// | ||
+ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||