This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-8 [24 Jul 2017 15:21] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:electronics:electronics-lab-8 [25 Jun 2020 22:07] (current) – external edit 127.0.0.1 | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: Stabilized current source (BJT) ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 24: | Line 24: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 1 KHz triangle wave with 3 volt amplitude and 1.5V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the collector of Q2. | + | {{: |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The waveform generator should be configured for a 1 KHz triangle wave with 3 volt amplitude | ||
===== Procedure: ===== | ===== Procedure: ===== | ||
The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the collector of transistor Q< | The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the collector of transistor Q< | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
+ | |||
+ | **Resources: | ||
+ | * LTSpice files: [[downgit> | ||
===== Questions: ===== | ===== Questions: ===== | ||
Line 46: | Line 61: | ||
The output current has a narrow peak. How could multiple copies of the peaking current source be combined to produce a much wider, flatter peak? | The output current has a narrow peak. How could multiple copies of the peaking current source be combined to produce a much wider, flatter peak? | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||