This shows you the differences between two versions of the page.
Next revisionBoth sides next revision | |||
university:courses:electronics:electronics-lab-8 [28 Oct 2012 19:32] – created Doug Mercer | university:courses:electronics:electronics-lab-8 [28 Oct 2012 19:36] – [Questions:] Doug Mercer | ||
---|---|---|---|
Line 40: | Line 40: | ||
Based on the delta V< | Based on the delta V< | ||
- | An exercise for the student | + | An exercise for the reader |
The output of the simple peaking current source is always less than the input current at the peak by a substantial fraction. What is that fraction and why? | The output of the simple peaking current source is always less than the input current at the peak by a substantial fraction. What is that fraction and why? | ||