This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-8 [24 Jul 2017 15:21] – change amplitude value to peak-peak Antoniu Miclaus | university:courses:electronics:electronics-lab-8 [29 Aug 2017 14:32] – add xy plot Antoniu Miclaus | ||
---|---|---|---|
Line 23: | Line 23: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
+ | |||
+ | {{: | ||
+ | |||
+ | <WRAP centeralign> | ||
The waveform generator should be configured for a 1 KHz triangle wave with 3 volt amplitude and 1.5V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the collector of Q2. | The waveform generator should be configured for a 1 KHz triangle wave with 3 volt amplitude and 1.5V offset. The input of scope channel 2 (2+) is used to measure the stabilized output current at the collector of Q2. | ||
Line 29: | Line 33: | ||
The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the collector of transistor Q< | The zero gain amplifier can be used to create a stabilized current source. Because the voltage seen at the collector of transistor Q< | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
===== Questions: ===== | ===== Questions: ===== |