Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:courses:electronics:electronics-lab-6m [23 Mar 2017 16:07] – [Materials:] Doug Merceruniversity:courses:electronics:electronics-lab-6m [25 Jun 2020 22:07] (current) – external edit 127.0.0.1
Line 1: Line 1:
-====== Activity 6M. NMOS as a Current Mirror ======+====== ActivityNMOS as a Current Mirror ======
  
 ===== Objective: ===== ===== Objective: =====
Line 21: Line 21:
  
 <WRAP centeralign> Figure 1 NMOS Current mirror test circuit </WRAP> <WRAP centeralign> Figure 1 NMOS Current mirror test circuit </WRAP>
 +
 +{{ :university:courses:electronics:a6m_nf2.png? |}}
 +<WRAP centeralign> Figure 2 NMOS Current mirror test circuit breadboard connection </WRAP>
  
 ===== Hardware Setup: ===== ===== Hardware Setup: =====
  
-In the current mirror configuration, the opamp serves as a virtual ground at the mirror input (gate) node to convert the voltage steps from AWG W2 output ) into current steps through the 1K? resistor. The drain voltage is swept using a ramp from AWG 1(output W1) set to 3V peak to peak with the offset to 1.5V. V<sub>DS</sub> of output device M<sub>2</sub> is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1K? resistor, R<sub>2</sub>.+In the current mirror configuration, the opamp serves as a virtual ground at the mirror input (gate) node to convert the voltage steps from AWG W1 output ) into current steps through the 1K? resistor. The drain voltage is swept using a ramp from AWG 1(output W1). Load the stairstep.csv file, set amplitude to 3V peak-to-peak with the offset to 1.5V. 
 +V<sub>DS</sub> of output device M<sub>2</sub> is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1K? resistor, R<sub>2</sub>.
 If you don't want to use the op-amp configuration the following simplified configuration can be used as well.  If you don't want to use the op-amp configuration the following simplified configuration can be used as well. 
  
 {{ :university:courses:electronics:a6m_f2.png?500 |}} {{ :university:courses:electronics:a6m_f2.png?500 |}}
  
-<WRAP centeralign> Figure simplified test configuration </WRAP>+<WRAP centeralign> Figure simplified test configuration </WRAP>
  
-===== Hardware Setup=====+{{ :university:courses:electronics:a6m_nf4.png? |}} 
 +<WRAP centeralign> Figure 4 Simplified test configuration breadboard connection </WRAP>
  
 ===== Procedure: ===== ===== Procedure: =====
Line 37: Line 42:
 Two identical transistors with the same gate to source voltage will have the same drain current I<sub>D</sub>. The second transistor, M<sub>2</sub>, in effect mirrors the current in the first, M<sub>1</sub>. Remembering the drain current to gate source voltage relationship for a MOS transistor: Two identical transistors with the same gate to source voltage will have the same drain current I<sub>D</sub>. The second transistor, M<sub>2</sub>, in effect mirrors the current in the first, M<sub>1</sub>. Remembering the drain current to gate source voltage relationship for a MOS transistor:
  
-{{ :university:courses:electronics:a6m_e1.png?250 |}}+{{ :university:courses:electronics:a6m_ne1.png? 250 |}}
  
 where K =μ<sub>n</sub>C<sub>ox</sub>/2<sub></sub> and λ can be taken as process technology constants.\\ where K =μ<sub>n</sub>C<sub>ox</sub>/2<sub></sub> and λ can be taken as process technology constants.\\
 Identical transistors by definition have the same W/L and process technology constants. In the simple current mirror, both transistors have the same V<sub>GS</sub>. Thus, both transistors will have the same I<sub>D</sub>. Since no current flows in the gate terminal of a FET I<sub>in</sub> = I<sub>out</sub>. Identical transistors by definition have the same W/L and process technology constants. In the simple current mirror, both transistors have the same V<sub>GS</sub>. Thus, both transistors will have the same I<sub>D</sub>. Since no current flows in the gate terminal of a FET I<sub>in</sub> = I<sub>out</sub>.
 +{{ :university:courses:electronics:a6m_nf5.png?500 |}}
 +<WRAP centeralign> Figure 5 Current Mirror waveform </WRAP>
  
 +<WRAP round download>
 +**Resources:**
 +  * Fritzing files: [[downgit>education_tools/tree/master/m2k/fritzing/mos_current_mirror_bb | mos_current_mirror_bb]]
 +  * LTspice files: [[downgit>education_tools/tree/master/m2k/ltspice/nmos_cur_mirror_ltspice | mos_current_mirror_ltspice]]
 +</WRAP>
 ===== Questions: ===== ===== Questions: =====
  
university/courses/electronics/electronics-lab-6m.1490281644.txt.gz · Last modified: 23 Mar 2017 16:07 by Doug Mercer