Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:courses:electronics:electronics-lab-6 [24 Aug 2018 04:48] – Added scopy screenshots to the activities Trecia Agoylo | university:courses:electronics:electronics-lab-6 [12 Jul 2019 13:06] – Pop Andreea |
---|
====== Activity 6. BJT Current Mirror ====== | ====== Activity: BJT Current Mirror ====== |
| |
===== Objective: ===== | ===== Objective: ===== |
<WRAP centeralign> Figure 1 Current mirror test circuit </WRAP> | <WRAP centeralign> Figure 1 Current mirror test circuit </WRAP> |
| |
{{ :university:courses:electronics:a6n_f2.png?500 |}} | {{ :university:courses:electronics:a6n_f2.png? |}} |
| |
<WRAP centeralign> Figure 2 Breadboard Connection of Current mirror test circuit </WRAP> | <WRAP centeralign> Figure 2 Breadboard Connection of Current mirror test circuit </WRAP> |
===== Hardware Setup: ===== | ===== Hardware Setup: ===== |
| |
In the current mirror configuration, the op amp serves as a virtual ground at the mirror input (base) node to convert the voltage steps from AWG 2 ( W2 output ) into current steps through the 1KΩ resistor. The collector voltage is swept using a ramp from AWG 1(output W1) set to 3V peak to peak with the offset to 1.5V. V<sub>CE</sub> of output device Q<sub>2</sub> is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1KΩ resistor, R<sub>2</sub>. | In the current mirror configuration, the op amp serves as a virtual ground at the mirror input (base) node to convert the voltage steps from AWG 2 ( W2 output ) into current steps through the 1KΩ resistor. The collector voltage is swept using a ramp from AWG 1(output W1). Load the stairstep.csv file, set amplitude to 1.5 (3V peak to peak) with the offset to 1.5V. |
| V<sub>CE</sub> of output device Q<sub>2</sub> is measured differentially by scope inputs 1+, 1-. The mirror output current is measured by scope inputs 2+. 2- across 1KΩ resistor, R<sub>2</sub>. |
If you don't want to use the op-amp configuration the following simplified configuration can be used as well. | If you don't want to use the op-amp configuration the following simplified configuration can be used as well. |
| |
<WRAP centeralign> Figure 3 Alt, Simple current mirror test circuit </WRAP> | <WRAP centeralign> Figure 3 Alt, Simple current mirror test circuit </WRAP> |
| |
{{ :university:courses:electronics:a6n_f4.png?500 |}} | {{ :university:courses:electronics:a6n_f4.png? |}} |
| |
<WRAP centeralign> Figure 4 Breadboard Connection of Simple current mirror test circuit </WRAP> | <WRAP centeralign> Figure 4 Breadboard Connection of Simple current mirror test circuit </WRAP> |
| |
=====Hardware Setup===== | =====Hardware Setup===== |
{{ :university:courses:electronics:a6n_f7.png?500 |}} | {{ :university:courses:electronics:a6n_f7.png? |}} |
| |
<WRAP centeralign> Figure 7 Breadboard Connection of Current Mirror with Base Current Compensation </WRAP> | <WRAP centeralign> Figure 7 Breadboard Connection of Current Mirror with Base Current Compensation </WRAP> |
<WRAP centeralign> Figure 9 Wilson current mirror </WRAP> | <WRAP centeralign> Figure 9 Wilson current mirror </WRAP> |
=====Hardware Setup===== | =====Hardware Setup===== |
{{ :university:courses:electronics:a6n_f10.png?500 |}} | {{ :university:courses:electronics:a6n_f10.png? |}} |
| |
<WRAP centeralign> Figure 10 Breadboard Connection of Wilson current mirror </WRAP> | <WRAP centeralign> Figure 10 Breadboard Connection of Wilson current mirror </WRAP> |
<WRAP centeralign> Figure 12 Widlar current mirror </WRAP> | <WRAP centeralign> Figure 12 Widlar current mirror </WRAP> |
=====Hardware Setup===== | =====Hardware Setup===== |
{{ :university:courses:electronics:a6n_f13.png?500 |}} | {{ :university:courses:electronics:a6n_f13.png? |}} |
| |
<WRAP centeralign> Figure 13 Breadboard Connection of Widlar current mirror </WRAP> | <WRAP centeralign> Figure 13 Breadboard Connection of Widlar current mirror </WRAP> |
| |
=====Hardware Setup===== | =====Hardware Setup===== |
{{ :university:courses:electronics:a6n_f16.png?500 |}} | {{ :university:courses:electronics:a6n_f16.png? |}} |
| |
<WRAP centeralign> Figure 16 Breadboard Connection of Low input head room mirror </WRAP> | <WRAP centeralign> Figure 16 Breadboard Connection of Low input head room mirror </WRAP> |
| |
Ideally the collector of PNP Q<sub>3</sub> would be connected to some negative voltage with respect to ground. Try connecting the collector of Q<sub>3</sub> to the negative board supply Vn. What happens? Can the input node of the mirror get even closer to ground now? | Ideally the collector of PNP Q<sub>3</sub> would be connected to some negative voltage with respect to ground. Try connecting the collector of Q<sub>3</sub> to the negative board supply Vn. What happens? Can the input node of the mirror get even closer to ground now? |
| |
| <WRAP round download> |
| **Resources:** |
| * Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/bjt_current_mirror_bb | bjt_current_mirror_bb]] |
| * LTspice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/bjt_current_mirror_ltspice | bjt_current_mirror_ltspice]] |
| </WRAP> |
| |
**Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]** | **Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]** |